NFC Tap App FW upgrade demo not working
Hi,
Fast Transfer Mode data transaction and image transactions are working ok, but firmware upgrade and some other functionalities (like stopwatch transfer) are not working in Android NFC Tap Application...
I'm using:
- ST25DV-Discovery kit with FW v1.1.2
- Android NFC Tap Application v3.2.0 (ST25SDK v1.6.0).
Debugging into NFC Tap App, I note that the problem is that ST25DV tag didn't response to addressed mode FTM Write Command (RF Protocol request message flag set to addressable transaction, and tag UID used in message transaction. Request flags - 0x22; address flag set to '1'). Also, no GPO event is fired, the Tag is not placing the data into the Mailbox:
...
this = DecorView@c70cd2c[ST25DVFirmwareUpdateDemoActivity]
D/Iso15693CustomCommand: ==> Send readDynConfig command: 22 ad 02 06 0c 1a 05 00 25 02 e0 0d
D/Iso15693CustomCommand: Response: 00 01
D/Iso15693CustomCommand: ==> Send writeMsg command: 22 aa 02 06 0c 1a 05 00 25 02 e0 08 08 01 00 00 04 12 34 56 78
D/Iso15693CustomCommand: ==> Send readDynConfig command: 22 ad 02 06 0c 1a 05 00 25 02 e0 0d
D/Iso15693CustomCommand: Response: 00 01
...
D/Iso15693CustomCommand: ==> Send writeMsg command: 22 aa 02 06 0c 1a 05 00 25 02 e0 08 08 01 00 00 04 12 34 56 78
D/Iso15693CustomCommand: ==> Send readDynConfig command: 22 ad 02 06 0c 1a 05 00 25 02 e0 0d
D/Iso15693CustomCommand: Response: 00 01
D/Iso15693CustomCommand: ==> Send writeMsg command: 22 aa 02 06 0c 1a 05 00 25 02 e0 08 08 01 00 00 04 12 34 56 78
D/Iso15693CustomCommand: ==> Send readDynConfig command: 22 ad 02 06 0c 1a 05 00 25 02 e0 0d
D/Iso15693CustomCommand: Response: 00 01
...At Android App code function "int sendSimpleData(byte command)", if I replace the write to MB function:
response = mST25DVTag.writeMailboxMessage(size + SIMPLE_HEADER_SIZE, frame);To force stop using adressed request, 0x02 (address flag set to '0'):
response = mST25DVTag.writeMailboxMessage(size + SIMPLE_HEADER_SIZE, frame, Iso15693Command.HIGH_DATA_RATE_MODE);I can get FW upgrade and stopwatch functionalities working properly:
...
D/View: [Warning] assignParent to null: this = DecorView@11b3f91[ST25DVFirmwareUpdateDemoActivity]
D/Iso15693CustomCommand: Response: 00 01
D/Iso15693CustomCommand: ==> Send writeMsg command: 02 aa 02 08 08 01 00 00 04 12 34 56 78
D/Iso15693CustomCommand: Response: 00
D/Iso15693CustomCommand: ==> Send readDynConfig command: 22 ad 02 06 0c 1a 05 00 25 02 e0 0d
D/Iso15693CustomCommand: Response: 00 43
D/Iso15693CustomCommand: ==> Send readMsgLength command: 22 ab 02 06 0c 1a 05 00 25 02 e0
D/Iso15693CustomCommand: Response: 00 04
D/Iso15693CustomCommand: ==> Send readMsg command: 22 ac 02 06 0c 1a 05 00 25 02 e0 00 04
D/Iso15693CustomCommand: Response: 00 08 01 00 00 00
D/ViewRootImpl[Toast]: hardware acceleration = true , fakeHwAccelerated = false, sRendererDisabled = false, forceHwAccelerated = false, sSystemRendererDisabled = false
D/Surface: Surface::allocateBuffers(this=0x7531ee5000)
D/Surface: Surface::connect(this=0x7531ee5000,api=1)
D/Iso15693CustomCommand: ==> Send readDynConfig command: 22 ad 02 06 0c 1a 05 00 25 02 e0 0d
D/Iso15693CustomCommand: Response: 00 41
D/Iso15693CustomCommand: ==> Send writeMsg command: 02 aa 02 f8 04 00 00 01 00 01 cc c4 01 f4 00 01 ec 58 2f 01 20 9d 01 0a 08 e1 4c 0a 08 a9 34 0a 08 25 41 0a 08 ed 13 0a 08 89 62 0a 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 99 60 0a 08 81 14 0a 08 00 00 00 00 03 4d 0a 08 79 61 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 b7 01 0a 08 21 17 0a 08 b7 01 0a 08 b7 01 0a 08
D/Iso15693CustomCommand: Response: 00
...
D/Iso15693CustomCommand: ==> Send writeMsg command: 02 aa 02 f8 04 00 00 01 00 01 cc c4 01 f4 00 0a ec 3a 46 ff f7 bf fe 32 46 bd e8 f0 41 00 f0 5c b8 00 00 f0 3f c1 f3 0a 52 c1 f3 13 01 40 f2 ff 33 41 f4 80 11 9a 42 02 da 00 20 01 46 70 47 40 f2 33 43 9a 42 a2 f2 33 42 02 dc 52 42 ff f7 5b be 00 f0 42 b8 30 b5 04 1e 71 f1 00 04 04 db 4f f0 00 44 40 42 64 eb 01 01 14 1e 73 f1 00 04 05 db 1c 46 4f f0 00 43 52 42 63 eb 04 03 8b 42 08 bf 82 42 30 bd 30 b5 04 1e 71 f1 00 04 04 db 4f f0 00 44 40 42 64 eb 01 01 14 1e 73 f1 00 04 05 db 1c 46 4f f0 00 43 52 42 63 eb 04 03 99 42 08 bf 90 42 30 bd 06 4c 07 4d 06 e0 e0 68 40 f0 01 03 94 e8 07 00 98 47 10 34 ac 42 f6 d3 ff f7 42 fc 8c ca 0b 08 ac ca 0b 08 20 2a 04 db 20 3a 00 fa 02 f1 00 20 70 47 91 40 c2 f1 20 03 20 fa 03 f3 19 43 90 40 70 47 20 2a 06 db cb 17
D/Iso15693CustomCommand: Response: 00
D/Iso15693CustomCommand: ==> Send writeMsg command: 02 aa 02 f8 04 00 00 01 00 01 cc c4 01 f4 00 0b ec 20 3a 41 fa 02 f0 43 ea e0 73 06 e0 41 fa 02 f3 d0 40 c2 f1 20 02 91 40 08 43 19 46 70 47 70 b5 8c 18 10 f8 01 5b 15 f0 07 03 01 d1 10 f8 01 3b 2a 11 06 d1 10 f8 01 2b 03 e0 10 f8 01 6b 01 f8 01 6b 5b 1e f9 d1 2b 07 05 d4 00 23 52 1e 0d d4 01 f8 01 3b fa e7 10 f8 01 3b cb 1a 92 1c 03 e0 13 f8 01 5b 01 f8 01 5b 52 1e f9 d5 a1 42 d8 d3 00 20 70 bd 4a 49 10 b5 d1 f8 04 23 22 f4 40 32 c1 f8 04 23 d1 f8 04 23 43 68 1a 43 c1 f8 04 23 01 68 4a 68 22 f4 80 72 4a 60 01 68 4a 68 03 69 42 ea 03 22 4a 60 01 68 4a 68 22 f0 40 72 4a 60 01 68 4a 68 83 68 1a 43 4a 60 01 68 8a 68 22 f4 00 62 8a 60 01 68 8a 68 c3 68 1a 43 8a 60 81 6a 6f f0 70 62 d1 42 01 68 8a 68 22 f0 70 62 8a 60 01 68 8a 68 0c d0 83 6a 1a 43 8a 60
D/Iso15693CustomCommand: Response: 00
...Summarizing:
Send writeMsg command not working:
[22 aa 02 06 0c 1a 05 00 25 02 e0 08 08 01 00 00 04 12 34 56 78]
RequestFlags: 22 (address_flag is set to 1 and data rate flag set to 1)
CMD: aa (writeMsg)
IC_MFG_CODE: 02
UID: 06 0c 1a 05 00 25 02 e0 (address_flag is set to 1)
MSG_LEN: 08
MSG_DATA: 08 01 00 00 04 12 34 56 78
No Response from Tag!
Send writeMsg command working:
[02 aa 02 08 08 01 00 00 04 12 34 56 78]
RequestFlags: 02 (address_flag is set to 0 and data rate flag set to 1)
CMD: aa (writeMsg)
IC_MFG_CODE: 02
UID: None (address_flag is 0)
MSG_LEN: 08
MSG_DATA: 08 01 00 00 04 12 34 56 78
Response from Tag: 00What can be the reason that ST25DV is not responding to addressed commands?
As documentation said, the tag didn't response if the message didn't contains the correct tag UID:

Maybe UID byte order (LSB/MSB) in Write Message is inverted and tag expects the other order?
Could it be a reader (smartphone) incompatibility in ISO-15963 for address mode transactions (I use the same reader device all the time)?
Sounds strange to me that no body report this problem before, maybe I miss something...
Regards.