NFC03A1 with Raspberry Pi 4, tag not detecting
HW : Raspberry PI 4 with NFC03A1 board connected to SPI
SW : Linux_RFAL_st25r95_v2.0.4.tar.gz
we built and we are able to run on the Rpi board, poller example
issue :
ISO1444A tag not detected
SPI seems to be working, we observed IDN command responds with the details as per the datasheet
IRQ_OUT also seems to be correct refer to log1.txt
rfalInitialize seems to be success. No errros
while ISO14443A tag detection we are observing err timeouts.. refer to log2.txt
pls advise