NUCLEO-NFC06A1
Good day.
I use devboard NFC06A1 with Nucleo-L053R8. Project from STM32CubeExpansion_NFC6_V1.0.0.
All works fine - via SPI. But when i choose i2C - i have a problem
- I changed resistorto select i2c
- add pull up resistor R116 and R117
- Add define RFAL_USE_I2C
4. change //HAL_NVIC_SetPriority(I2C1_EV_IRQn, 5, 5);
//HAL_NVIC_EnableIRQ(I2C1_EV_IRQn);
HAL_NVIC_SetPriority(I2C1_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(I2C1_IRQn);
Device was crash when call I2C_Enable_IRQ(hi2c, I2C_XFER_TX_IT); in stm32l0xx_hal_i2c.c
MCU freez in startup_stm32l053xx.s
I2C1_IRQHandler
I2C2_IRQHandler
SPI1_IRQHandler
SPI2_IRQHandler
USART1_IRQHandler
USART2_IRQHandler
RNG_LPUART1_IRQHandler
LCD_IRQHandler
USB_IRQHandler
B . ;crash in current line
ENDP
ALIGNWhat a mistake here ?