Skip to main content
Visitor II
October 23, 2018
Solved

NXP NTAG compatibility with CR95HF

  • October 23, 2018
  • 1 reply
  • 821 views

As I understand it, NXP's NTAG family (NTAG 210u, NTAG 21x) are fully compliant NFC Forum Type 2 and ISO/IEC14443 Type A devices, and as such, they should work with the CR95HF. However, these tags have additional features, like an originality signature, that areoutside the scope of the standards. Are these additional features compatible as well, or are they only supported by NXP readers?

    This topic has been closed for replies.
    Best answer by Peter Boringer

    ​Hi sir,

    According to the NXP specification, even if the command are outside the scope of the standards, this feature should be accessible with the CR95HF if you program the appropriate command with the suggested protocol. The CR95HF will only do the transfer all has to be pre processed by the micro-controller.

    Regards

    PB

    1 reply

    Visitor II
    November 13, 2018

    ​Hi sir,

    According to the NXP specification, even if the command are outside the scope of the standards, this feature should be accessible with the CR95HF if you program the appropriate command with the suggested protocol. The CR95HF will only do the transfer all has to be pre processed by the micro-controller.

    Regards

    PB