Optimizing current for tag detection (ST25R95)
Hello,
I am trying to optimize the current consumption in tag detection mode for my battery reader (based on ST25R95).
I have followed the application note for keeping current at minimum with tag detection as suggestred below:
https://community.st.com/s/question/0D53W00000BsxIdSAJ/approach-for-low-power-design
1)
In the AN (section 2.4 "Using LFO frequency settings to reduce power consumption") says the the LFO at 4kHz will reduce energy, but I have tested and energy is not reduced.
As far as I know the LFO clk is the same for different frequencies, the change is for the presecaler.
My question: ¿Does a lower LFO freqquency really save energy?
2)
I know the tuning for the antenna is very important for reaching good performances at reading level, but I would like to know how a good tuning impact on the current consumption.
3)
Other option I am assessing is to decrease the OSC and DAC start time (recommended to be 3 ms). How risky is to decrease this time under 3ms?
----
FYI:
I am currently using RF bursts of 2,3us and I am having a consumption of 50uA (as expected). I can not reduce this time because it wouldn´t detect tags otherwise.
POWER at 3,3V (both main and TX).
Any suggestion will be welcome.
Regards, Ramon.