Password Protection for T2T Tags with ST25R200
Hi all,
I am using ST25R200 and NTAG215 from NXP. I configured RFAL to use T2T and NFCA
#define RFAL_FEATURE_LISTEN_MODE false /*!< Enable/Disable RFAL support for Listen Mode */
#define RFAL_FEATURE_WAKEUP_MODE true /*!< Enable/Disable RFAL support for the Wake-Up mode */
#define RFAL_FEATURE_LOWPOWER_MODE true /*!< Enable/Disable RFAL support for the Low Power mode */
#define RFAL_FEATURE_NFCA true /*!< Enable/Disable RFAL support for NFC-A (ISO14443A) */
#define RFAL_FEATURE_NFCB false /*!< Enable/Disable RFAL support for NFC-B (ISO14443B) */
#define RFAL_FEATURE_NFCF false /*!< Enable/Disable RFAL support for NFC-F (FeliCa) */
#define RFAL_FEATURE_NFCV false /*!< Enable/Disable RFAL support for NFC-V (ISO15693) */
#define RFAL_FEATURE_T1T false /*!< Enable/Disable RFAL support for T1T (Topaz) */
#define RFAL_FEATURE_T2T true /*!< Enable/Disable RFAL support for T2T */
#define RFAL_FEATURE_T4T false /*!< Enable/Disable RFAL support for T4T */
#define RFAL_FEATURE_ST25TB false /*!< Enable/Disable RFAL support for ST25TB */
#define RFAL_FEATURE_ST25xV false /*!< Enable/Disable RFAL support for ST25TV/ST25DV */
#define RFAL_FEATURE_DYNAMIC_ANALOG_CONFIG false /*!< Enable/Disable Analog Configs to be dynamically updated (RAM) */
#define RFAL_FEATURE_DPO false /*!< Enable/Disable RFAL Dynamic Power Output support */
#define RFAL_FEATURE_ISO_DEP true /*!< Enable/Disable RFAL support for ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_POLL true /*!< Enable/Disable RFAL support for Poller mode (PCD) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_LISTEN false /*!< Enable/Disable RFAL support for Listen mode (PICC) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_NFC_DEP false /*!< Enable/Disable RFAL support for NFC-DEP (NFCIP1/P2P) */
So far detecting the Tag and reading and writing works just fine by using:
rfalT2TPollerWrite
rfalT2TPollerReadHowever, I am not sure how I can use the password protection feature from the nfc tag. I would like to be able to set a password and then to read and write from memory using the set password. What API Methods would I use for that? I am quite confused with all the different types and Feature configurations. I only want to use and support T2T tags, which should be able to handle password protection.