Problem with NFC Tag detection using ST25R95
We have designed a a custom PCB with a custom antenna using ST25R95 NFC Tag reader, also the antenna tuning has been done. We found an issue during our testing, at our production site the tags are not getting detected but the same PCBs are working fine in our office.
We have observed that the AC mains supply is stable at both locations but the mains frequency isn’t stable at the production site. We are using a standard power adapter with input rating 110-240V 50/60Hz Output 5V 4A. Can the mains frequency variation lead to NFC chip not reading tags or it has to do something with the environment (EMI)?
Also the DC voltage on the ST_R0 Pin is around 7.8V in both the environments (office as well as production site) indicating that the RF field is on if I'm not mistaken.