Problems communicating to the ST25R95 using SPI -- No communication from IC
My setup is as follows:
- ST25R95 is in a QFN32 chip holder (https://www.amazon.com/gp/product/B01N6NF3ME/), which allows me to test with test leads to a breadboard.
- Powering chip (VPS and VTx) with 3.3V with a bench power supply, which reads a constant 0.25-0.26 Amps current when the IC is powered. If I disconnect the Tx power, it pulls 0.18 Amps.
- SPI interface, SSI_0, SSI_1, IRQ_IN, IRQ_OUT from a Raspberry PI 4B+. I've tied grounds from bench supply and raspberry pi to avoid floating grounds.
- SPI clock is 1 MHz.
- A Wurth 27.12 MHz crystal oscillator (model number 830014948B) with 10 pf capacitors. (Tested with and without this attached.)
- Logic Analyzer is a Digilent Analog Discovery 2 (https://digilent.com/shop/analog-discovery-2-100ms-s-usb-oscilloscope-logic-analyzer-and-variable-power-supply/) running Waveforms software (https://digilent.com/shop/software/digilent-waveforms/).
- Communication software Python 3 script and SPI using spidev. spidev ensures proper SS (Select) control. It goes low before the command and returns high after commands are sent. Logic Analyzer shows this code is working properly.
After 8 days of trying, I've not been able to get any communication out of the IC. I purchased 3 of these and have swapped out a fresh IC in case the 1st was fried.
My script setups the GPIO pins of the Raspberry Pi as well as the SPI interface. When power is supplied, the script::
- sets SSI_0 to 1 and SSI_1 to 0
- I have a buttons that:
- sets IRQ_IN to low for 0.5 seconds
- opens the spi communications
- sends 0x00, 0x02 (plus other settings) for 15693 protocol
- sends 0x01 (IDN) for requesting info
- sends 0x02.to read 13 bytes (also attempted reading 1 byte at a time)
- has an input box to allow me to enter commands not programmed in my buttons.
The documentation is confusing in that it says 0x00 is required to send a command. However, none of the examples show this. An IDN request should be 0x00, 0x01, 0x00 according to the written instructions. I never get any response on the IRQ_OUT pin, so I also tried polling. Even after a second between each poll request, I still could not get any response from the chip.
The examples are more confusing than helpful. The IDN command examples says to issue "0x0100" That is 256 , but I did try that as well. I also tried 0x00 and this command. And as I said, I also tried 0x00, 0x01, and 0x00.
I would like to see some form of output from the IC. What am I doing wrong? I would assume the crystal osc is not required just for communication testing, but I did also try with this.
I am more than willing to send pictures of the setup and my script. Please help.