read multiple RFID 14334A tags
What are the best chip/settings to read multiple RFID 14334A tags? What should I look at when selecting chip?
I need to create a reader that needs to read playing cards (14334A) from the table.
Currently, I have a setup with AS3910 chip. It works fine while 1-2 cards go through its field simultaneously.
1) First issue
If I stack one card on another it can read only up to 2 cards like that. When I stack 3 cards it can't.
2) Second issue
If cards (2-16) are in its field from the start it usually then can read just one card and sometimes more. (No idea why. Even if I leave the cards in the same place)
So I wonder what is responsible for these limitations? Is it the wrong settings, old chip, wrong protocol, or just the physical limitations of RFID technology?
Thanks!