read the inventory of ISO15693 tag with ST25R3916
Dircet_Command(SET_Default);
Register_Write(IO_configuration1, 0x04); // IO Configuration1 register Write 0x04
Register_Write(IO_configuration2, 0x84); // IO Configuration2 register Write 0x84
Register_Write(Bit_rate_definition, 0x00); // Bit Rate Defintion register Write 0x00
Register_Write(Stream_mode_definition, 0x18); // Stream Mode definition register Write 0x18
Register_Write(Mode_defintion,0x74); // Mode Defintion register Write 0x74
Register_Write(Operation_control,0xC8); // Operation control register Write 0xC8
FIFO_load(FIFO_TX,CMD_BUF); //FIFO Buf Wirte CMD_BUF
(Write to the register as long as the buffer length)
Register_Write(Number_of_transmitted_bytes1,len);
Register_Write(Number_of_transmitted_bytes2,len);
Dircet_Command(Transmit_without_CRC); //Send data stored in FIFO Buff
static uint8_t TXReadUID[22]=
{0x21,0x20,0x08,0x20,0x02,0x08,0x02,0x02,0x02,0x02,0x02,0x02,0x02,0x20,0x08,0x80,0x80,0x20,0x20,0x02,0x02,0x04};
uint8_t message_length = 22;
This command is the CMD of ISO15693, which converts the Inventory request command to the 4_1 format.
while(1){
if(Register_Read(Main_interrupt) & 0x10){
FIFO_Read = 0x9F;
HAL_SPI_TransmitReceive(&hspi2,FIFO_Read,rx_buffer,fifo_len,1000);
}
}
Receive Data = [ 11 A2 88 28 22 45 84 84 10 41 08 11 42 48 08 21 11 84 88 28 85 A2 48 44 10 ]