rfalST25xVPollerGenericWriteMessage() fails writing to mailbox
Hi,
I have some code for reading/writing to a mailbox from the ST25R3916B transceiver to a ST25DV04KC-I tag. The read passes but the write fails every time.
My reading function looks like this ...
bool nfc_read_mailbox(void)
{
uint8_t pointer;
uint8_t reg;
uint8_t pwd[8] = {0, 0, 0, 0, 0, 0, 0, 0};
uint8_t pwdLen = 8;
uint8_t pwdNum = 0;
uint8_t msgLen;
ReturnCode err;
uint16_t rcvLen;
uint8_t rxBuf[256];
bool result = false;
memset(&rxBuf[0], 0x00, sizeof(rxBuf));
/* Open RF configuration security session */
err = rfalST25xVPollerPresentPassword(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pwdNum, pwd, pwdLen);
if (err == RFAL_ERR_NONE)
{
/* set MB_MODE to 1: Enabling fast transfer mode is authorized.*/
pointer = ST25DV04K_SYSTEM_CONFIG_MB_MODE;
reg = ST25DV04K_REG_MB_MODE_FTM_AUTHORIZED;
err = rfalST25xVPollerWriteConfiguration(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pointer, reg);
if (err == RFAL_ERR_NONE)
{
/* set MB_EN to 1: Enable FTM. Read, update and write */
pointer = ST25DV04K_DYN_REG_MB_CTRL;
err = rfalST25xVPollerFastReadDynamicConfiguration(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pointer, ®);
if (err == RFAL_ERR_NONE)
{
reg |= ST25DV04K_REG_MB_CTRL_DYN_MB_EN;
err = rfalST25xVPollerFastWriteDynamicConfiguration(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pointer, reg);
if (err == RFAL_ERR_NONE)
{
/* Read Msg Len */
err = rfalST25xVPollerReadMessageLength(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, &msgLen);
if (err == RFAL_ERR_NONE)
{
/* Read Msg */
err = rfalST25xVPollerReadMessage(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, 0, 0, rxBuf, sizeof(rxBuf), &rcvLen);
if (err == RFAL_ERR_NONE)
{
result = true;
}
}
}
}
}
}
return result;
}
My writing function looks like this ...
bool nfc_write_mailbox(char *message)
{
uint8_t pointer;
uint8_t reg;
uint8_t pwd[8] = {0, 0, 0, 0, 0, 0, 0, 0};
uint8_t pwdLen = 8;
uint8_t pwdNum = 0;
uint8_t msgLen;
ReturnCode err;
uint16_t rcvLen;
uint8_t txBuf[256];
bool result = false;
memset(&txBuf[0], 0x00, sizeof(txBuf));
sprintf(txBuf, "%s", message);
/* Open RF configuration security session */
err = rfalST25xVPollerPresentPassword(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pwdNum, pwd, pwdLen);
if (err == RFAL_ERR_NONE)
{
/* set MB_MODE to 1: Enabling fast transfer mode is authorized.*/
pointer = ST25DV04K_SYSTEM_CONFIG_MB_MODE;
reg = ST25DV04K_REG_MB_MODE_FTM_AUTHORIZED;
err = rfalST25xVPollerWriteConfiguration(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pointer, reg);
if (err == RFAL_ERR_NONE)
{
/* set MB_EN to 1: Enable FTM. Read, update and write */
pointer = ST25DV04K_DYN_REG_MB_CTRL;
err = rfalST25xVPollerFastReadDynamicConfiguration(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pointer, ®);
if (err == RFAL_ERR_NONE)
{
reg |= ST25DV04K_REG_MB_CTRL_DYN_MB_EN;
err = rfalST25xVPollerFastWriteDynamicConfiguration(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, pointer, reg);
if (err == RFAL_ERR_NONE)
{
/* Write Msg */
//err = rfalST25xVPollerFastWriteMessage(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, strlen(txBuf), (const uint8_t *)&txBuf, (uint8_t *)&txBuf, sizeof(txBuf));
err = rfalST25xVPollerWriteMessage(RFAL_NFCV_REQ_FLAG_DEFAULT, NULL, strlen(txBuf), (const uint8_t*) &txBuf, (uint8_t*) &txBuf, sizeof(txBuf) );
if (err == RFAL_ERR_NONE)
{
result = true;
}
}
}
}
}
return result;
}
The failure happens in the call to rfalTransceiveBlockingTxRx() in rfalST25xVPollerGenericWriteMessage().
The tx works (line 5 below) but the rx fails (line 6 below) with a timeout (ret=RFAL_ERR_TIMEOUT).
ReturnCode rfalTransceiveBlockingTxRx( uint8_t* txBuf, uint16_t txBufLen, uint8_t* rxBuf, uint16_t rxBufLen, uint16_t* actLen, uint32_t flags, uint32_t fwt )
{
ReturnCode ret;
RFAL_EXIT_ON_ERR( ret, rfalTransceiveBlockingTx( txBuf, txBufLen, rxBuf, rxBufLen, actLen, flags, fwt ) );
ret = rfalTransceiveBlockingRx();
/* Convert received bits to bytes */
if( actLen != NULL )
{
*actLen = rfalConvBitsToBytes(*actLen);
}
return ret;
}
Do I have the write sequence correct or am I missing something?
Thanks