RFID distance issue with ST25R3916B
We are building an RFID reader. I copied the schematic and RF + antenna from the X-NUCLEO-NFC08A1. The design works, but I have an issue with the reading distance.
Some RFID tags are detected over 5 cm away, while others need to be placed less than 1 cm from the reader antenna. Where should I look to solve this issue?
I tried some commercial readers, and they all read tags from the same distances. I cut the antenna from the NUCLEO-NFC08A1 and replaced the one on our reader, but the result was the same. I also replaced all the RF components on our reader with those on the NUCLEO, and there was no change.
I tried many things related to RF design and antenna matching, but nothing helped. How can I achieve consistent reading of all RFID tags at the same distance, and ensure that the distance is more than 3 cm?
I'm now suspecting the variable capacitors or some settings in the ST25R3916B.
Best
Dejan