SDK for ST25RU3993 EVAL
Is there any SDK and sample code for the ST25RU3993 EVAL board? I would like to know what the API is from the PC side and of course some sample code (C# preferred).
Is there any SDK and sample code for the ST25RU3993 EVAL board? I would like to know what the API is from the PC side and of course some sample code (C# preferred).
Hello Bchri.1,
yes, the problem is that we currently have two different version of the FW. One that is able to communicate with the GUI (V1.8.6) and one that can be operated by the STUHFL_demo sample source code (v1.9.0). The low level functionality is the same for both version, but the communciation layer has changed for these two FW version.
We will soon release a V2.0.0 of the FW, GUI and STUHFL_demo were all components are compatible.
For the moment to run the STUHFL_demo you need to flash the v1.9.0 FW from the package. You could use KEIL or TrueStudio to build, flash and debug the FW.
BR
Nick
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.