Solved
Solved: Another mistake in M24SR datasheet
Posted on April 02, 2014 at 12:27
Hi,
as [DEAD LINK /public/STe2ecommunities/memories/Lists/M24SR%20Series/Flat.aspx?RootFolder=/public/STe2ecommunities/memories/Lists/M24SR%20Series/M24SR%20-%20mistake%20in%20table%2067%20Datasheet&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000ED3A9C6410AD9C49B9619F3BDE3D015F¤tviews=84]somebody commented, there is a mistake in the M24SR's datasheet. In Figure ''NDEF tag Application Select Command'' a 0x04 is missing between 0xA4 and 0x00. In addition, there is another one in the last byte of the time flow. Last bytes have to be 0xF1 0x09. These two errors are present at least in my version of M24SR02-Y. Have a nice day. #m24sr #an4433 #datasheet-error #ds #m24sr