Skip to main content
Visitor II
December 2, 2020
Solved

Source code for CR95HF?

  • December 2, 2020
  • 1 reply
  • 719 views

I am looking for the source code of CR95HF.DLL.

The project successfully implements bidirectional comms between CH95HF hardware (which is based on the DEMO-CR95HF-A board) with a M24SR02-Y in the target device. We use CR95HF.DLL V1.2 with various Delphi-developed applications.

A problem has been observed when the applications are used in countries that do not use US English environments. The nul-terminated paraters used in the DLL calls appear to be an issue. Data appears to be modified IN the DLL with single characters appearing as two bytes (i.e. unicode representations)

My feeling is that modifying the DLL would solve this problem.

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    thanks for using the CR95HF product. The source code of the CR95HF DLL will be provided to you in private.

    Rgds

    BT

    1 reply

    Technical Moderator
    December 2, 2020

    Hi,

    thanks for using the CR95HF product. The source code of the CR95HF DLL will be provided to you in private.

    Rgds

    BT