ST-Link V2 Utility cannot connect to SmarTag1 target.
Upgraded ST-Link to V2.J29.M18 STM32 Debug+Mass storage.
STM32 ST-LINK Utility is v4.2.0.0 USBDriver v5.0.3.0 CLI.exe v3.2.0.0
Removed both ST link jumpers .
Fresh CR2032 battery installed on STEVAL-SmarTag1
Connected directly on SWD (pin 1 correctly aligned)
Message Can not connect to target!
ST-Link V2 is connected to Nucleo L476 board.
ST-Link does connect to this board when ST-links reinstalled.
I have also tried a separated ST-Link V2. Also no connection to SmartTag1
How do I connect to the STEVAL-SmarTag1 to change firmware from default?