ST25DV and energy harvesting
Hi to all.
I should make an application with NFC where the entire circuit is powered by energy harvesting.
For this reason I thought of using the ST25DV and I have already purchased the ST25DV_Discovery_C1 and ST25DV_Discovery_C6
On these discovery I closed ST3 to connect 3.3V with EH, I connected the pins of GND and 3.3V of connector J1 to an oscilloscope to monitor the voltage supplied, and then I approached the cell phone to the discovery with the active NFC (and with the application of the open ST).
I have set (as from the manual) the EH_MODE register to 0 and therefore I have once again allonato and reapproached the mobile.
What I expected to find from the oscilloscope is a continuous voltage whereas what I find is a signal varying between approximately + 500mV and about -500mV, except for an initial transnitory in which the voltage rises up to about 30V but is extinguished in about 50ms.
Furthermore this behavior occurs both with EH_MODE at 0 and with EH_MODE at 1, except for the initial transient that occurs only when EH_MODE is at 0.
Is it right or am I doing something wrong? Is energy harvesting only the initial transient or even the variable signal between + 500mV and - 500mV?
I also noticed that the EH_CTRL_Dyn register has in any case the first three bits (EH_EN, EH_ON and FIELD_ON) always at 1.
I hope I was clear.
Thanks in advance.
Luca G.