ST25DV password protection
I activated the area1 password protection with password 1. I saw that the default password is "0". Is there a way to change the password 1 over the I2C or is it only possible to change it from NFC side?
I saw that all RF_PWD witch can be configurated to the areas can be change over RF in secure session. But also the secure password is default "0". So I have to configurate the chip with NFC to work in the mass? Or how can I deal with it over I2C to be configurated default for our use?