ST25DV04K – RF password and factory reset
Hello everyone,
I’m currently working with the ST25DV04K chip and I’ve noticed two points that are a bit confusing:
There doesn’t seem to be any way to change the RF passwords via I²C.
I couldn’t find any command that allows a full factory reset (including resetting the passwords).
My questions are:
Is this really the case, or am I missing some undocumented/hidden command?
If the passwords are set via I²C and cannot be changed anymore, doesn’t this risk making the device unusable in case of a configuration mistake?
Is there any recommended method from ST to bring the chip back to a “clean” state without replacing it?
Thanks in advance to anyone who can clarify these points.