Skip to main content
Visitor II
August 8, 2022
Solved

ST25DV64KC GPO pulse when i2c write EEPROM

  • August 8, 2022
  • 2 replies
  • 710 views

 Hi

I'm using ST25DV64KC, my I2C host is STM32G474

There are two problem, need support. 

Please see detail. Thank you!

1. I would like GPO generates a pulse when i2c write EEPROM(user memory)

but it doesn't work, the GPO always output Low

I have confirmed, the GPO_EN = 1 in GPO1 register, I2C_WRITE_EN = 1 in GPO2 register

2.Can I use ST "NFC Tap" app for testing? How? Could you provide more detail information to me?

EX. NFC Tap app send some RF command, and use I2C to read the data.

    This topic has been closed for replies.
    Best answer by France Berthelot

    Hello

    For #2, you can use Mobile apps and register feature (static/Dynamic) to configure GPO.

    Regards,FB

    2 replies

    Visitor II
    August 16, 2022

    As for question #1, did you remember to connect a pull-up resistor to the GPO output? A value of 10K would do the job.

    Nir

    ST Employee
    August 22, 2022

    Hello

    For #2, you can use Mobile apps and register feature (static/Dynamic) to configure GPO.

    Regards,FB