ST25R Obtain RSSI of multiple tags
Hello everyone,
I am working on a project that requires identifying the RSSI of all surrounding tags.
If "tag 6361" is not placed, the remaining three tags can be recognized and their RSSI can be obtained. However, after placing "tag 6361", only "tag 6361" can be recognized, and the other three tags cannot communicate.
The RSSI of the four tags is: tag "66E9" has an RSSI of 101, tag "635A" has an RSSI of 28, tag "681D" has an RSSI of 73, and tag "675A" has an RSSI of 1736.
May I ask how to make these four labels recognized simultaneously?