Skip to main content
Visitor II
January 30, 2025
Solved

ST25R100 Poller tag discovery

  • January 30, 2025
  • 6 replies
  • 2043 views

Hi there

Starting point

I am currently working on porting our NFC implementation from the ST25R3916 to the ST25R100.

We will also replace our current library (Lib-NFC & ST_25r & RFAL) and use the current libraries (RFAL and NDEF) from ST.

For the migration I currently use a NUCLEO-U575ZI-Q board and two NFC shields (X-NUCLEO-NFC06A1 with the current ST25R3916 and X-NUCLEO-NFC09A1 with the new ST25R100).

I already successfully migrated our implementation to the new library. I'm able to poll for NFCA and NFCV tags using the X-NUCLEO-NFC06A1 shield.

Issue Description

  • With the X-NUCLEO-NFC09A1 shield connected, I'm not able to discover any NFCA or NFCV tags. Communication with the ST25R100 seems to work just fine (no errors).
  • gNfcDev.state enters states: RFAL_NFC_STATE_START_DISCOVERY, RFAL_NFC_STATE_POLL_TECHDETECT and RFAL_NFC_STATE_LISTEN_TECHDETECT (which indicates that no tag has been detected)

 

May you have a clue why ST25R100 sees nothing?

Any support is highly appreciated.

Best,

Stefan

 

Files & Info

rfal_platform.h (same config for both ST25 derivates):

//===================================================================
// GLOBAL DEFINES
//===================================================================

#define ST25R_SS_PIN NULL ///< GPIO pin used for ST25R SPI SS
#define ST25R_SS_PORT NULL ///< GPIO port used for ST25R SPI SS port

#define ST25R_INT_PIN NULL ///< GPIO pin used for ST25R External Interrupt
#define ST25R_INT_PORT GpioCfg_ptNfcIrqDevice ///< GPIO port used for ST25R External Interrupt

#define PLATFORM_LED_A_PIN NULL ///< GPIO pin used for LED A
#define PLATFORM_LED_A_PORT NULL ///< GPIO port used for LED A
#define PLATFORM_LED_B_PIN NULL ///< GPIO pin used for LED B
#define PLATFORM_LED_B_PORT NULL ///< GPIO port used for LED B
#define PLATFORM_LED_F_PIN NULL ///< GPIO pin used for LED F
#define PLATFORM_LED_F_PORT NULL ///< GPIO port used for LED F
#define PLATFORM_LED_V_PIN NULL ///< GPIO pin used for LED V
#define PLATFORM_LED_V_PORT NULL ///< GPIO port used for LED V
#define PLATFORM_LED_AP2P_PIN NULL ///< GPIO pin used for LED AP2P
#define PLATFORM_LED_AP2P_PORT NULL ///< GPIO port used for LED AP2P

#define PLATFORM_USER_BUTTON_PIN NULL ///< GPIO pin user button
#define PLATFORM_USER_BUTTON_PORT NULL ///< GPIO port user button

//===================================================================
// GLOBAL MACROS
//===================================================================

#define platformProtectST25RComm() System_vEnterCriticalSection() ///< Protect unique access to ST25R communication channel
#define platformUnprotectST25RComm() System_vExitCriticalSection() ///< Unprotect unique access to ST25R communication channel

#define platformProtectST25RIrqStatus() System_vEnterCriticalSection() ///< Protect unique access to ST25R communication channel
#define platformUnprotectST25RIrqStatus() System_vExitCriticalSection() ///< Unprotect unique access to ST25R communication channel

#define platformLedOff( port, pin ) platformGpioClear(port, pin) ///< Clear the GPIO
#define platformLedOn( port, pin ) platformGpioSet(port, pin) ///< Set the GPIO
#define platformLedToggle( port, pin ) platformGpioToggle(port, pin) ///< Toggle the GPIO

#define platformGpioSet( port, pin ) HAL_GPIO_WritePin(port, pin, GPIO_PIN_SET) ///< Turns the given GPIO High
#define platformGpioClear( port, pin ) HAL_GPIO_WritePin(port, pin, GPIO_PIN_RESET) ///< Turns the given GPIO Low
#define platformGpioToggle( port, pin ) HAL_GPIO_TogglePin(port, pin) ///< Toogles the given GPIO
#define platformGpioIsHigh( port, pin ) ((Gpio_eGetLevel(port) == Gpio_LEVEL_HIGH) ? true : false) ///< Checks if the given GPIO definition is High
#define platformGpioIsLow( port, pin ) ((Gpio_eGetLevel(port) == Gpio_LEVEL_LOW) ? true : false) ///< Checks if the given GPIO definition is Low

#define platformTimerCreate( t ) (platformGetSysTick() + t) ///< Create a timer with the given time (ms)
#define platformTimerIsExpired( timer ) ((int32_t)(timer - platformGetSysTick()) < 0) ? true : false ///< Checks if the given timer is expired
#define platformDelay( t ) System_vBusyWaitMs( t ) ///< Performs a delay for the given time (ms)

#define platformGetSysTick() SupTimer_u32GetCounter() ///< Get System Tick ( 1 tick = 1 ms)

#define platformAssert( exp ) ASSERT_TRUE( exp , "") ///< Asserts whether the given expression is true
#define platformErrorHandle() Err_HANDLE_REUSABLE_ERROR(0, "RFAL_ERR"); ///< Global error handle trap


#ifdef RFAL_USE_I2C

#define platformI2CTx( txBuf, len, last, txOnly ) i2cSequentialTx((uint16_t)0xA0, (uint8_t *)(txBuf), (len), last, txOnly ) /*!< I2C Transmit */
#define platformI2CRx( txBuf, len ) i2cSequentialRx((uint16_t)0xA0, rxBuf, len ) ///< I2C Receive
#define platformI2CStart() ///< I2C Start condition
#define platformI2CStop() ///< I2C Stop condition
#define platformI2CRepeatStart() ///< I2C Repeat Start
#define platformI2CSlaveAddrWR(add) ///< I2C Slave address for Write operation
#define platformI2CSlaveAddrRD(add) ///< I2C Slave address for Read operation

#else /* RFAL_USE_I2C */

#define platformSpiSelect() SPI_vCsEnable(SpiCfg_ptST25R3916SpiDevice) ///< Enable CS PIN
#define platformSpiDeselect() SPI_vCsDisable(SpiCfg_ptST25R3916SpiDevice) ///< Disable CS PIN
#define platformSpiTxRx( txBuf, rxBuf, len ) SPI_vTxRx(SpiCfg_ptST25R3916SpiDevice, txBuf, rxBuf, len) ///< Interface to SPI tx and rx function

#endif /* RFAL_USE_I2C */

#define platformLog(...) ///< Log method (currently not used)



//===================================================================
// GLOBAL VARIABLES
//===================================================================

extern uint8_t globalCommProtectCnt; ///< Global Protection Counter provided per platform - instantiated in main.c



//===================================================================
// RFAL FEATURES CONFIGURATION
//===================================================================

#define RFAL_FEATURE_LISTEN_MODE false /*!< Enable/Disable RFAL support for Listen Mode */
#define RFAL_FEATURE_WAKEUP_MODE true /*!< Enable/Disable RFAL support for the Wake-Up mode */
#define RFAL_FEATURE_LOWPOWER_MODE true /*!< Enable/Disable RFAL support for the Low Power mode */
#define RFAL_FEATURE_NFCA true /*!< Enable/Disable RFAL support for NFC-A (ISO14443A) */
#define RFAL_FEATURE_NFCB true /*!< Enable/Disable RFAL support for NFC-B (ISO14443B) */
#define RFAL_FEATURE_NFCF false /*!< Enable/Disable RFAL support for NFC-F (FeliCa) */
#define RFAL_FEATURE_NFCV true /*!< Enable/Disable RFAL support for NFC-V (ISO15693) */
#define RFAL_FEATURE_T1T true /*!< Enable/Disable RFAL support for T1T (Topaz) */
#define RFAL_FEATURE_T2T true /*!< Enable/Disable RFAL support for T2T */
#define RFAL_FEATURE_T4T true /*!< Enable/Disable RFAL support for T4T */
#define RFAL_FEATURE_ST25TB true /*!< Enable/Disable RFAL support for ST25TB */
#define RFAL_FEATURE_ST25xV true /*!< Enable/Disable RFAL support for ST25TV/ST25DV */
#define RFAL_FEATURE_DYNAMIC_ANALOG_CONFIG false /*!< Enable/Disable Analog Configs to be dynamically updated (RAM) */
#define RFAL_FEATURE_DPO false /*!< Enable/Disable RFAL Dynamic Power Output support */
#define RFAL_FEATURE_ISO_DEP true /*!< Enable/Disable RFAL support for ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_POLL true /*!< Enable/Disable RFAL support for Poller mode (PCD) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_LISTEN false /*!< Enable/Disable RFAL support for Listen mode (PICC) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_NFC_DEP false /*!< Enable/Disable RFAL support for NFC-DEP (NFCIP1/P2P) */

#define RFAL_FEATURE_ISO_DEP_IBLOCK_MAX_LEN 256U /*!< ISO-DEP I-Block max length. Please use values as defined by rfalIsoDepFSx */
#define RFAL_FEATURE_NFC_DEP_BLOCK_MAX_LEN 254U /*!< NFC-DEP Block/Payload length. Allowed values: 64, 128, 192, 254 */
#define RFAL_FEATURE_NFC_RF_BUF_LEN 258U /*!< RF buffer length used by RFAL NFC layer */

#define RFAL_FEATURE_ISO_DEP_APDU_MAX_LEN 512U /*!< ISO-DEP APDU max length. Please use multiples of I-Block max length */
#define RFAL_FEATURE_NFC_DEP_PDU_MAX_LEN 512U /*!< NFC-DEP PDU max length. */



//===================================================================
// RFAL CUSTOM SETTINGS
//===================================================================
// Custom analog configs are used to cope with Automatic Antenna Tuning (AAT)
// that are optimized differently for each board.

#define RFAL_ANALOG_CONFIG_CUSTOM ///< Use Custom Analog Configs when defined

// Empty macros (not used)
#define platformProtectWorker() ///< Protect RFAL Worker/Task/Process from concurrent execution on multi thread platforms
#define platformUnprotectWorker() ///< Unprotect RFAL Worker/Task/Process from concurrent execution on multi thread platforms
#define platformIrqST25RPinInitialize() ///< Initializes ST25R IRQ pin
#define platformIrqST25RSetCallback( cb ) ///< Sets ST25R ISR callback
#define platformLedsInitialize() ///< Initializes the pins used as LEDs to outputs
#define platformTimerDestroy( timer ) ///< Stops and released the given timer


#endif /* SYSTEM_RFAL_PLATFORM_H_ */

 

The function that initializes the RFAL library (and predefines the discovery parameters):

bool_t NfcInterface_bInit(const NfcInterface_EventHandler_t pxEventHandler, const NfcInterface_GetSystemUpTime_t pxGetSystemUptime, uint8_t u8RxConfReg3Value, uint8_t u8DetectMode)
{

	// register handler/Adapters
	tEnv.pxEventHandler = pxEventHandler;
	tEnv.pxGetSysUpTimeAdapter = pxGetSystemUptime;
	tEnv.u16Rssi = 0;

	// Initialize RFAL NFC discovery parameters
	rfalNfcDefaultDiscParams(&tEnv.tRfalNfcDiscoverParam);
	tEnv.tRfalNfcDiscoverParam.devLimit = NFC_MAX_DEVICE_COUNT; // 2 devices
	tEnv.tRfalNfcDiscoverParam.totalDuration = RFAL_NFC_WORKER_DEVICE_DISCOVERY_TIMEOUT_MS; // 1000ms
	tEnv.tRfalNfcDiscoverParam.techs2Find = RFAL_NFC_POLL_TECH_A | RFAL_NFC_POLL_TECH_V;
	tEnv.tRfalNfcDiscoverParam.notifyCb = vRfalNfcEvHandler; // This handler is mandatory to avoid that the library autoselects the first tag (even if multiple tags have been discovered)

	// Initialize RFAL library
	ReturnCode eRfalErr = rfalNfcInitialize();
	LOG_ERROR_IF(eRfalErr != RFAL_ERR_NONE, "NFC initialization failed: error = %u", eRfalErr);
	RETURN_IF(eRfalErr != RFAL_ERR_NONE, FALSE);

#if defined(ST25R3916) || defined(ST25R3916B)
	// disable AAT (automatic antenna tuning)
	uint8_t u8RegValue = 0u;
	st25r3916ReadRegister(ST25R3916_REG_IO_CONF2, &u8RegValue);
	u8RegValue &= ~(1<<5);
	st25r3916WriteRegister(ST25R3916_REG_IO_CONF2, u8RegValue);
	// set gain boost based on setting
	st25r3916WriteRegister(ST25R3916_REG_RX_CONF3, u8RxConfReg3Value);
#endif

	NfcInterface_vSetPower(TRUE);
	return true;
}

 

The function that runs the discovery:

(annotation: The actual discovery is performed synchronously... by calling rfalNfcWorker until the expected rfal nfc state has been reached. This is because of our legacy API that expects synchronous functions.)

bool_t NfcInterface_bRfalDiscoverTags(bool_t bForceReDiscover)
{
	rfalNfcState eRfalNfcState = rfalNfcGetState();
	bool_t bAlreadyDiscovered = (eRfalNfcState == RFAL_NFC_STATE_POLL_SELECT) || (eRfalNfcState == RFAL_NFC_STATE_ACTIVATED) || (eRfalNfcState == RFAL_NFC_STATE_LISTEN_TECHDETECT)? TRUE : FALSE;
	LOG_ERROR_IF((bForceReDiscover != TRUE) && (bAlreadyDiscovered != TRUE), "Tag Discovery failed: eRfalNfcState %u", eRfalNfcState);
	RETURN_IF((bForceReDiscover != TRUE) && (bAlreadyDiscovered != TRUE), FALSE);

	if(bForceReDiscover == TRUE)
	{
		NfcInterface_vResetDeviceList();

		// Perform Tag discovery
		ReturnCode eRfalErr = rfalNfcDiscover(&tEnv.tRfalNfcDiscoverParam);
		LOG_ERROR_IF(eRfalErr != RFAL_ERR_NONE, "Failed to initiate NFC Discovery: Return Code %u", eRfalErr);
		RETURN_IF(eRfalErr != RFAL_ERR_NONE, 0);

		// Run worker until device discovery is finished
		eRfalNfcState = eRfalRunNfcWorker(RFAL_NFC_WORKER_DEVICE_DISCOVERY_TIMEOUT_MS,
				RFAL_NFC_STATE_POLL_SELECT, // State entered if multiple tags have been discovered
				RFAL_NFC_STATE_ACTIVATED, // State entered if one tag has been discovered
				RFAL_NFC_STATE_LISTEN_TECHDETECT); // State enteren if no tag has been discovered
	}
	else{} // Dont initiate discovery if not already done

	LOG_DEBUG("State after tag discovery: %u", eRfalNfcState);

	bool_t bSuccess = (eRfalNfcState == RFAL_NFC_STATE_POLL_SELECT) || (eRfalNfcState == RFAL_NFC_STATE_ACTIVATED) || (eRfalNfcState == RFAL_NFC_STATE_LISTEN_TECHDETECT)? TRUE : FALSE;
	LOG_ERROR_IF(!bSuccess, "Tag Discovery failed: eRfalNfcState %u", eRfalNfcState);

	return bSuccess;
}

 

static rfalNfcState eRfalRunNfcWorker(uint32_t u32TimeoutMs, rfalNfcState eTargetState1, rfalNfcState eTargetState2, rfalNfcState eTargetState3)
{
	const uint32_t u32TimeoutThreshold = SupTimer_u32GetCounter() + u32TimeoutMs;

	do
	{
		rfalNfcWorker();
	} while((SupTimer_u32GetCounter() < u32TimeoutThreshold) &&
			(rfalNfcGetState() != eTargetState1) && (rfalNfcGetState() != eTargetState2) && (rfalNfcGetState() != eTargetState3));

	return rfalNfcGetState();
}

 

    This topic has been closed for replies.
    Best answer by Ulysses HERNIOSUS

    Hi,

    I think you are using compile time flag RFAL_ANALOG_CONFIG_CUSTOM and supply some custom analog config file for 3916. Please disable/remove RFAL_ANALOG_CONFIG_CUSTOM and then the R100 should start working.

    BR, Ulysses

    6 replies

    Technical Moderator
    January 30, 2025

    Hi Stefan,

     

    baseline points:

    1. How is the ST25R100 reset pin connected?
    2. Please enable ST25R_SELFTEST
    3. Can you observe if an RF field is emitted? Either LED based field detector or oscilloscope with a loop of the GND cable to the tip
    4. Please share a logic analyzer trace with SPI and INT pin.

    BR, Ulysses

    Stef2Author
    Visitor II
    February 3, 2025

    Hello Ulysses

    Thanks for your support (and sorry for the delay).

    • Reset pin is connected to GND
    • Ok, I'll enable selftest and see what info I can get out of it
    • Yes, I observe an RF Filed, as soon as I start the discovery procedure (see image below)
    • I'll do a trace and post it (have access to a logic analyzer tomorrow)

    Stef2_0-1738563306961.png

     

    Stef2Author
    Visitor II
    February 3, 2025

    Ok... I've enabled ST25R_SELFTEST (first taught that's kind of a chip testmode, but its additional testcode which is part of the st25rx specific RFAL).

    That Test runs through without any error...

     

    Stef2_1-1738564999695.png

     

    Stef2Author
    Visitor II
    February 4, 2025

    I've now captured the SPI communication and IRQ pin... (didn't yet try to analyze it... I'll do now)

    Many thanks for your support.

    Best, Stefan

     

    Initialization Sequence (MOSI/MISO): 
    
    0x60/0x00 0xBF/0x00 0x00/0xA9 0x29/0xFF 0x33/0xFF 0xA9/0xFF 0x00/0x33 0x29/0xFF 0x00/0xFF 0x28/0xFF 0x08/0xFF 0xE4/0xFF
     
    0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x02 0x3B/0x00 0x02/0x00 0x28/0x00 0x00/0x00 0x80/0x00 0x00/0x00 0x80/0x00 0x00/0x00 0x00/0x00 0x02/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x01 0x3B/0xFF 0x03/0xFF 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x7F 0x80/0xFF 0x00/0x02 0x39/0x00 0xFF/0x00 0x3A/0x00 0xFF/0x00 0x3B/0x00 0xFF/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x00 0xFC/0x00 0x02/0x00 0x00/0x00 0x80/0x00 0x00/0x02 0x00/0x00 0x07/0x00 0x81/0x00 0x00/0x00 0x01/0x00 0x18/0x00 0x81/0x00 0x00/0x18 0x01/0x00 0x38/0x00 0xA8/0x00 0x00/0x00 0x81/0x00 0x00/0x38 0x80/0x00 0x00/0x03 0x00/0x00 0x33/0x00 0x81/0x00 0x00/0x38 0x3B/0x00 0xEF/0x00 0x68/0x00
    
    0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x100x80/0x00 0x00/0x33 0x00/0x00 0x03/0x000x80/0x00 0x00/0x03 0x00/0x00 0x33/0x00

    Stef2_0-1738657333820.png

     

     

    Discovery Sequence (MOSI/MISO): 
    
    0x60/0x00 0xBF/0x00 0x00/0xA9 0x29/0xFF 0x33/0xFF 0xA9/0xFF 0x00/0x33 0x29/0xFF 0x00/0xFF 0x28/0xFF 0x08/0xFF 0xE4/0xFF
    
    0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x02 0x3B/0x00 0x02/0x00 0x28/0x00 0x00/0x00 0x80/0x00 0x00/0x00 0x80/0x00 0x00/0x00 0x00/0x00 0x02/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x01 0x3B/0xFF 0x03/0xFF 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x7F 0x80/0xFF 0x00/0x02 0x39/0x00 0xFF/0x00 0x3A/0x00 0xFF/0x00 0x3B/0x00 0xFF/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x00 0xFC/0x00 0x02/0x00 0x00/0x00 0x80/0x00 0x00/0x02 0x00/0x00 0x07/0x00 0x81/0x00 0x00/0x00 0x01/0x00 0x18/0x00 0x81/0x00 0x00/0x18 0x01/0x00 0x38/0x00 0xA8/0x00 0x00/0x00 0x81/0x00 0x00/0x38 0x80/0x00 0x00/0x03 0x00/0x00 0x33/0x00 0x81/0x00 0x00/0x38 0x3B/0x00 0xEF/0x00 0x68/0x00
    
    0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x10 0x3B/0x00 0xFF/0x00 0x8F/0x00 0x00/0x78 0x80/0x00 0x00/0x33 0x00/0x00 0x03/0x00
    
    0x80/0x00 0x00/0x03 0x80/0x00 0x00/0x03 0x80/0x00 0x00/0x03 0x00/0x00 0x33/0x00 0x80/0x00 0x00/0x33 0x12/0x00 0x01/0x00 0xCC/0x00 0x00/0x00 0x8A/0x00 0x00/0x4A 0xCC/0x00 0x00/0x00 0x92/0x00 0x00/0x01 0x92/0x00 0x00/0x01 0x83/0x00 0x00/0x00 0x03/0x00 0x04/0x00 0xA8/0x00 0x00/0x00 0x28/0x00 0x70/0x00 0x83/0x00 0x00/0x04 0x03/0x00 0x00/0x00 0x8B/0x00 0x00/0x07 0x0B/0x00 0x08/0x00 0x8C/0x00 0x00/0xAA 0x0C/0x00 0x2D/0x00 0x8D/0x00 0x00/0x03 0x0D/0x00 0x00/0x00 0x8E/0x00 0x00/0x30 0x0E/0x00 0x00/0x00 0xCC/0x00 0x00/0x00 0x4C/0x00 0x51/0x00 0xCD/0x00 0x00/0x00 0x99/0x00 0x00/0x48 0x80/0x00 0x00/0x33 0x80/0x00 0x00/0x33
    
    0x80/0x00 0x00/0x33 0x96/0x00 0x00/0x3C 0x16/0x00 0x3D/0x00 0x80/0x00 0x00/0x33 0x9B/0x00 0x00/0x21 0x1C/0x00 0x0E/0x00 0x9E/0x00 0x00/0x00 0x1F/0x00 0x00/0x00 0x20/0x00 0x23/0x00 0x91/0x00 0x00/0x00 0x62/0x00 0x66/0x00 0x21/0x00 0x02/0x00 0x22/0x00 0xC8/0x00 0x9E/0x00 0x00/0x00 0x1E/0x00 0x10/0x00 0x93/0x00 0x00/0x60 0x13/0x00 0x00/0x00 0x96/0x00 0x00/0x3D 0x16/0x00 0x39/0x00 0x88/0x00 0x00/0xCC 0x9E/0x00 0x00/0x10 0x39/0x00 0xD1/0x00 0x3A/0x00 0xB0/0x00 0x35/0x00 0x07/0x00 0x34/0x00 0x00/0x00 0x5F/0x00 0x26/0x00 0x6A/0x00 0xBC/0x00 0x00/0x02 0x00/0x00 0x00/0x00 0xBC/0x00 0x00/0x00 0x00/0x40 0x00/0x00 0x93/0x00 0x00/0x00 0x13/0x00 0x60/0x00 0x96/0x00 0x00/0x39 0x16/0x00 0x3D/0x00 0x88/0x00 0x00/0xCC 0x96/0x00 0x00/0x3D 0x16/0x00 0x3C/0x00 0x12/0x00 0x05/0x00 0x8A/0x00 0x00/0x4A 0x8B/0x00 0x00/0x08 0x0B/0x00 0x13/0x00 0x8C/0x00 0x00/0x2D 0x8D/0x00 0x00/0x00 0x8E/0x00 0x00/0x00 0xCC/0x00 0x00/0x00 0x4C/0x00 0x13/0x00 0xCD/0x00 0x00/0x00 0x4D/0x00 0x01/0x00 0x92/0x00 0x00/0x05 0x92/0x00 0x00/0x05 0x83/0x00 0x00/0x00 0x03/0x00 0x04/0x00 0xA8/0x00 0x00/0x70 0x83/0x00 0x00/0x04 0x03/0x00 0x00/0x00 0x99/0x00 0x00/0x48 0x80/0x00 0x00/0x33 0x80/0x00 0x00/0x33
    
    0x96/0x00 0x00/0x3C 0x16/0x00 0x3D/0x00 0x80/0x00 0x00/0x33 0x9B/0x00 0x00/0x21 0x1C/0x00 0x41/0x00 0x9E/0x00 0x00/0x10 0x1F/0x00 0x00/0x00 0x20/0x00 0x8A/0x00 0x39/0x00 0x91/0x00 0x91/0x00 0x00/0x00 0x62/0x00 0x66/0x00 0x21/0x00 0x01/0x00 0x22/0x00 0x84/0x00 0x9E/0x00 0x00/0x10 0x93/0x00 0x00/0x60 0x96/0x00 0x00/0x3D 0x88/0x00 0x00/0xCC 0x9E/0x00 0x00/0x10 0x35/0x00 0x18/0x00 0x34/0x00 0x00/0x00 0x5F/0x00 0x26/0x00 0x01/0x00 0x00/0x00 0x6A/0x00
    
    0xBC/0x00 0x00/0x02 0x00/0x00 0x00/0x00 0xBC/0x00 0x00/0x80 0x00/0x40 0x00/0x00 0x93/0x00 0x00/0x60 0x96/0x00 0x00/0x3D 0x88/0x00 0x00/0xCC 0x39/0x00 0xD1/0x00 0x96/0x00 0x00/0x3D 0x16/0x00 0x3C/0x00 0x83/0x00 0x00/0x00 0x80/0x00 0x00/0x33 0x00/0x00 0x03/0x00
    
    0x60/0x00 0xBF/0x00 0x00/0xA9 0x29/0xFF 0x33/0xFF 0xA9/0xFF 0x00/0x33 0x29/0xFF 0x00/0xFF 0x28/0xFF 0x08/0xFF 0xE4/0xFF
    
    0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x02 0x3B/0x00 0x02/0x00 0x28/0x00 0x00/0x00 0x80/0x00 0x00/0x00 0x80/0x00 0x00/0x00 0x00/0x00 0x02/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x01 0x3B/0xFF 0x03/0xFF 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x3F 0x8F/0xFF 0x00/0x7F 0x80/0xFF 0x00/0x02 0x39/0x00 0xFF/0x00 0x3A/0x00 0xFF/0x00 0x3B/0x00 0xFF/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x00 0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x00 0xFC/0x00 0x02/0x00 0x00/0x00 0x80/0x00 0x00/0x02 0x00/0x00 0x07/0x00 0x81/0x00 0x00/0x00 0x01/0x00 0x18/0x00 0x81/0x00 0x00/0x18 0x01/0x00 0x38/0x00 0xA8/0x00 0x00/0x00 0x81/0x00 0x00/0x38 0x80/0x00 0x00/0x03 0x00/0x00 0x33/0x00 0x81/0x00 0x00/0x38 0x3B/0x00 0xEF/0x00 0x68/0x00
    
    0xBC/0x00 0x00/0x00 0x00/0x00 0x00/0x100x80/0x00 0x00/0x33 0x00/0x00 0x03/0x00

    Stef2_1-1738657420832.png

     

     

    Technical Moderator
    February 4, 2025

    Hi,

    please provide the Salae trace file.

    Rgds

    BT

     

    Stef2Author
    Visitor II
    February 4, 2025

    Here it is...

    Stef2Author
    Visitor II
    February 4, 2025

    Maybe HEX format is better...

    Technical Moderator
    February 4, 2025

    just provide the .sal file

    Stef2Author
    Visitor II
    February 4, 2025

    Ok...

    Technical Moderator
    February 4, 2025

    Hi,

    in order to decode the SPI frame being sent, the SPI  Chip Select (CS or SS or BSS)  is also needed in the trace. Can you connect it to your logic analyzer and provide a new trace?

    Rgds

    BT

    Stef2Author
    Visitor II
    February 4, 2025

    Ok... heres the .sal with BSS :)

    Stef2Author
    Visitor II
    February 4, 2025

    Again... (sorry, but im not certain if I had placed the NFCV tag in the field)...

    Technical Moderator
    February 4, 2025

    Hi,

    I think you are using compile time flag RFAL_ANALOG_CONFIG_CUSTOM and supply some custom analog config file for 3916. Please disable/remove RFAL_ANALOG_CONFIG_CUSTOM and then the R100 should start working.

    BR, Ulysses

    Stef2Author
    Visitor II
    February 4, 2025

    Great!Stef2_0-1738672934429.png

    That was the issue... tag detection works now. I didn't have this flag on my radar, as the related file was located in another corner of our project structure.

    I am very grateful for your valuable support! Thank you very much.

    Kind Regards,

    Stefan