ST25R100 with STM32G0 Freeze in rfalWorker
I am currently trying to use the NFC09A1 together with an STM32G0. I am having multiple issues.
I am using ST25NFC_Embedded_Lib_ST25R200_1.8.0_2
I setup the platform and SPI. SPI communication is working properly. I checked the signals and I can also properly read the chips ID in the rfalInit.
Basically i am initializing with
rfalNfcInitialize()and then doing something like this:
rfalNfcDiscoverParam discParam;
rfalNfcDefaultDiscParams(&discParam);
discParam.devLimit = 1;
discParam.techs2Find = RFAL_NFC_POLL_TECH_A;
if (rfalNfcDiscover(&discParam) != RFAL_ERR_NONE)
{
return Result::Error;
}
static rfalNfcDevice* nfcDevice;
while (true)
{
rfalNfcWorker();
HAL_Delay(500);
}On the SPI bus I can see traffic happening And also the Antenna seems to radiate a signal. However, after maybe 5-10 Cycles of the while loop the programm suddenly freezes. I seems that it gets stuck in this loop:
static ReturnCode rfalTransceiveRunBlockingTx( void )
{
ReturnCode ret;
do{
rfalWorker();
ret = rfalGetTransceiveStatus();
}
while( (rfalIsTransceiveInTx()) && (ret == RFAL_ERR_BUSY) );
if( rfalIsTransceiveInRx() )
{
return RFAL_ERR_NONE;
}
return ret;
}I am testing with an NXP NTAG215 which from my understanding should be NFC-A T2T, this is also the only configuration that I need working.
This is my rfal_platform. Where I also included the PIN setup:
/******************************************************************************
* @attention
*
* COPYRIGHT 2018 STMicroelectronics, all rights reserved
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied,
* AND SPECIFICALLY DISCLAIMING THE IMPLIED WARRANTIES OF MERCHANTABILITY,
* FITNESS FOR A PARTICULAR PURPOSE, AND NON-INFRINGEMENT.
* See the License for the specific language governing permissions and
* limitations under the License.
*
******************************************************************************/
/*! \file
*
* \author
*
* \brief Platform header file. Defining platform independent functionality.
*
*/
#ifndef RFAL_PLATFORM_H
#define RFAL_PLATFORM_H
#ifdef __cplusplus
extern "C" {
#endif
/*
******************************************************************************
* INCLUDES
******************************************************************************
*/
#include <stdint.h>
#include <stdbool.h>
#include <stdlib.h>
#include <limits.h>
#include <math.h>
#include "main.h"
#include "spi.h"
#include "timer.h"
#include "logger.h"
#include "stm32g0xx_hal.h"
#define ST25R200
#define B1_Pin GPIO_PIN_13
#define B1_GPIO_Port GPIOC
#define LED_FIELD_Pin GPIO_PIN_1
#define LED_FIELD_GPIO_Port GPIOA
#define LED_A_Pin GPIO_PIN_4
#define LED_A_GPIO_Port GPIOA
#define LED_B_Pin GPIO_PIN_0
#define LED_B_GPIO_Port GPIOB
#define LED5_Pin GPIO_PIN_10
#define LED5_GPIO_Port GPIOB
#define LED_V_Pin GPIO_PIN_8
#define LED_V_GPIO_Port GPIOA
#define ST25R_IRQ_Pin GPIO_PIN_0
#define ST25R_IRQ_GPIO_Port GPIOA
#define ST25R_IRQ_EXTI_IRQn EXTI0_1_IRQn
#define ST25R_RST_Pin GPIO_PIN_11
#define ST25R_RST_GPIO_Port GPIOB
#define SPI1_CS_Pin GPIO_PIN_12
#define SPI1_CS_GPIO_Port GPIOB
#define LED_RX_Pin GPIO_PIN_4
#define LED_RX_GPIO_Port GPIOB
/*
******************************************************************************
* GLOBAL DEFINES
******************************************************************************
*/
#define ST25R_SS_PIN SPI1_CS_Pin /*!< GPIO pin used for ST25R SPI SS */
#define ST25R_SS_PORT SPI1_CS_GPIO_Port /*!< GPIO port used for ST25R SPI SS port */
#define ST25R_INT_PIN ST25R_IRQ_Pin /*!< GPIO pin used for ST25R External Interrupt */
#define ST25R_INT_PORT ST25R_IRQ_GPIO_Port /*!< GPIO port used for ST25R External Interrupt */
#define ST25R_RESET_PIN ST25R_RST_Pin /*!< GPIO pin used for ST25R Reset */
#define ST25R_RESET_PORT ST25R_RST_GPIO_Port /*!< GPIO port used for ST25R Reset */
#ifdef LED_FIELD_Pin
#define PLATFORM_LED_FIELD_PIN LED_FIELD_Pin /*!< LED 1 GPIO pin used as field LED */
#endif
#ifdef LED_FIELD_GPIO_Port
#define PLATFORM_LED_FIELD_PORT LED_FIELD_GPIO_Port /*!< LED 1 GPIO port used as field LED */
#endif
#define PLATFORM_LED_A_PIN LED_A_Pin /*!< LED 2 GPIO pin used for LED A */
#define PLATFORM_LED_A_PORT LED_A_GPIO_Port /*!< LED 2 GPIO port used for LED A */
#define PLATFORM_LED_B_PIN LED_B_Pin /*!< LED 3 GPIO pin used for LED B */
#define PLATFORM_LED_B_PORT LED_B_GPIO_Port /*!< LED 3 GPIO port used for LED B */
#define PLATFORM_LED_F_PIN LED5_Pin /*!< LED 5 GPIO pin used for LED F */
#define PLATFORM_LED_F_PORT LED5_GPIO_Port /*!< LED 5 GPIO port used for LED F */
#define PLATFORM_LED_V_PIN LED_V_Pin /*!< LED 4 GPIO pin used for LED V */
#define PLATFORM_LED_V_PORT LED_V_GPIO_Port /*!< LED 4 GPIO port used for LED V */
#define PLATFORM_LED_AP2P_PIN LED5_Pin /*!< LED 5 GPIO pin used for LED AP2P */
#define PLATFORM_LED_AP2P_PORT LED5_GPIO_Port /*!< LED 5 GPIO port used for LED AP2P */
#define PLATFORM_USER_BUTTON_PIN B1_Pin /*!< GPIO pin user button */
#define PLATFORM_USER_BUTTON_PORT B1_GPIO_Port /*!< GPIO port user button */
/*
******************************************************************************
* GLOBAL MACROS
******************************************************************************
*/
#define platformProtectST25RComm() do{ globalCommProtectCnt++; __DSB();NVIC_DisableIRQ(ST25R_IRQ_EXTI_IRQn);__DSB();__ISB();}while(0) /*!< Protect unique access to ST25R communication channel - IRQ disable on single thread environment (MCU) ; Mutex lock on a multi thread environment */
#define platformUnprotectST25RComm() do{ if (--globalCommProtectCnt==0) {NVIC_EnableIRQ(ST25R_IRQ_EXTI_IRQn);} }while(0) /*!< Unprotect unique access to ST25R communication channel - IRQ enable on a single thread environment (MCU) ; Mutex unlock on a multi thread environment */
#define platformProtectST25RIrqStatus() platformProtectST25RComm() /*!< Protect unique access to IRQ status var - IRQ disable on single thread environment (MCU) ; Mutex lock on a multi thread environment */
#define platformUnprotectST25RIrqStatus() platformUnprotectST25RComm() /*!< Unprotect the IRQ status var - IRQ enable on a single thread environment (MCU) ; Mutex unlock on a multi thread environment */
#define platformLedOff( port, pin ) platformGpioClear(port, pin) /*!< Turns the given LED Off */
#define platformLedOn( port, pin ) platformGpioSet(port, pin) /*!< Turns the given LED On */
#define platformLedToggle( port, pin ) platformGpioToggle(port, pin) /*!< Toggles the given LED */
#define platformGpioSet( port, pin ) HAL_GPIO_WritePin(port, pin, GPIO_PIN_SET) /*!< Turns the given GPIO High */
#define platformGpioClear( port, pin ) HAL_GPIO_WritePin(port, pin, GPIO_PIN_RESET) /*!< Turns the given GPIO Low */
#define platformGpioToggle( port, pin ) HAL_GPIO_TogglePin(port, pin) /*!< Toggles the given GPIO */
#define platformGpioIsHigh( port, pin ) (HAL_GPIO_ReadPin(port, pin) == GPIO_PIN_SET) /*!< Checks if the given LED is High */
#define platformGpioIsLow( port, pin ) (!platformGpioIsHigh(port, pin)) /*!< Checks if the given LED is Low */
#define platformTimerCreate( t ) timerCalculateTimer(t) /*!< Create a timer with the given time (ms) */
#define platformTimerIsExpired( timer ) timerIsExpired(timer) /*!< Checks if the given timer is expired */
#define platformDelay( t ) HAL_Delay(t) /*!< Performs a delay for the given time (ms) */
#define platformGetSysTick() HAL_GetTick() /*!< Get System Tick ( 1 tick = 1 ms) */
#define platformAssert( exp ) assert_param( exp ) /*!< Asserts whether the given expression is true*/
#define platformErrorHandle() Error_Handler() /*!< Global error handle\trap */
#define platformSpiSelect() platformGpioClear(ST25R_SS_PORT, ST25R_SS_PIN)/*!< SPI SS\CS: Chip|Slave Select */
#define platformSpiDeselect() platformGpioSet(ST25R_SS_PORT, ST25R_SS_PIN) /*!< SPI SS\CS: Chip|Slave Deselect */
#define platformSpiTxRx( txBuf, rxBuf, len ) spiTxRx(txBuf, rxBuf, len) /*!< SPI transceive */
#define platformLog(...) logUsart(__VA_ARGS__) /*!< Log method */
/*
******************************************************************************
* GLOBAL VARIABLES
******************************************************************************
*/
extern uint8_t globalCommProtectCnt; /* Global Protection Counter provided per platform - instantiated in main.c */
/*
******************************************************************************
* RFAL FEATURES CONFIGURATION
******************************************************************************
*/
#define RFAL_FEATURE_LISTEN_MODE false /*!< Enable/Disable RFAL support for Listen Mode */
#define RFAL_FEATURE_WAKEUP_MODE true /*!< Enable/Disable RFAL support for the Wake-Up mode */
#define RFAL_FEATURE_LOWPOWER_MODE true /*!< Enable/Disable RFAL support for the Low Power mode */
#define RFAL_FEATURE_NFCA true /*!< Enable/Disable RFAL support for NFC-A (ISO14443A) */
#define RFAL_FEATURE_NFCB false /*!< Enable/Disable RFAL support for NFC-B (ISO14443B) */
#define RFAL_FEATURE_NFCF false /*!< Enable/Disable RFAL support for NFC-F (FeliCa) */
#define RFAL_FEATURE_NFCV false /*!< Enable/Disable RFAL support for NFC-V (ISO15693) */
#define RFAL_FEATURE_T1T false /*!< Enable/Disable RFAL support for T1T (Topaz) */
#define RFAL_FEATURE_T2T true /*!< Enable/Disable RFAL support for T2T */
#define RFAL_FEATURE_T4T false /*!< Enable/Disable RFAL support for T4T */
#define RFAL_FEATURE_ST25TB false /*!< Enable/Disable RFAL support for ST25TB */
#define RFAL_FEATURE_ST25xV false /*!< Enable/Disable RFAL support for ST25TV/ST25DV */
#define RFAL_FEATURE_DYNAMIC_ANALOG_CONFIG false /*!< Enable/Disable Analog Configs to be dynamically updated (RAM) */
#define RFAL_FEATURE_DPO false /*!< Enable/Disable RFAL Dynamic Power Output support */
#define RFAL_FEATURE_ISO_DEP true /*!< Enable/Disable RFAL support for ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_POLL true /*!< Enable/Disable RFAL support for Poller mode (PCD) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_LISTEN false /*!< Enable/Disable RFAL support for Listen mode (PICC) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_NFC_DEP false /*!< Enable/Disable RFAL support for NFC-DEP (NFCIP1/P2P) */
#define RFAL_FEATURE_ISO_DEP_IBLOCK_MAX_LEN 256U /*!< ISO-DEP I-Block max length. Please use values as defined by rfalIsoDepFSx */
#define RFAL_FEATURE_NFC_DEP_BLOCK_MAX_LEN 254U /*!< NFC-DEP Block/Payload length. Allowed values: 64, 128, 192, 254 */
#define RFAL_FEATURE_NFC_RF_BUF_LEN 258U /*!< RF buffer length used by RFAL NFC layer */
#define RFAL_FEATURE_ISO_DEP_APDU_MAX_LEN 512U /*!< ISO-DEP APDU max length. Please use multiples of I-Block max length */
#define RFAL_FEATURE_NFC_DEP_PDU_MAX_LEN 512U /*!< NFC-DEP PDU max length. */
/*
******************************************************************************
* RFAL CUSTOM SETTINGS
******************************************************************************
*/
#define platformTimerGetRemaining( timer ) (0U) /*!< Gets the remaining time until expiration */
#ifndef platformProtectST25RIrqStatus
#define platformProtectST25RIrqStatus() /*!< Protect unique access to IRQ status var - IRQ disable on single thread environment (MCU) ; Mutex lock on a multi thread environment */
#endif /* platformProtectST25RIrqStatus */
#ifndef platformUnprotectST25RIrqStatus
#define platformUnprotectST25RIrqStatus() /*!< Unprotect the IRQ status var - IRQ enable on a single thread environment (MCU) ; Mutex unlock on a multi thread environment */
#endif /* platformUnprotectST25RIrqStatus */
#ifndef platformProtectWorker
#define platformProtectWorker() /* Protect RFAL Worker/Task/Process from concurrent execution on multi thread platforms */
#endif /* platformProtectWorker */
#ifndef platformUnprotectWorker
#define platformUnprotectWorker() /* Unprotect RFAL Worker/Task/Process from concurrent execution on multi thread platforms */
#endif /* platformUnprotectWorker */
#ifndef platformIrqST25RPinInitialize
#define platformIrqST25RPinInitialize() /*!< Initializes ST25R IRQ pin */
#endif /* platformIrqST25RPinInitialize */
#ifndef platformIrqST25RSetCallback
#define platformIrqST25RSetCallback( cb ) /*!< Sets ST25R ISR callback */
#endif /* platformIrqST25RSetCallback */
#ifndef platformLedsInitialize
#define platformLedsInitialize() /*!< Initializes the pins used as LEDs to outputs */
#endif /* platformLedsInitialize */
#ifndef platformLedOff
#define platformLedOff( port, pin ) /*!< Turns the given LED Off */
#endif /* platformLedOff */
#ifndef platformLedOn
#define platformLedOn( port, pin ) /*!< Turns the given LED On */
#endif /* platformLedOn */
#ifndef platformLedToggle
#define platformLedToggle( port, pin ) /*!< Toggles the given LED */
#endif /* platformLedToggle */
#ifndef platformGetSysTick
#define platformGetSysTick() /*!< Get System Tick ( 1 tick = 1 ms) */
#endif /* platformGetSysTick */
#ifndef platformTimerDestroy
#define platformTimerDestroy( timer ) /*!< Stops and released the given timer */
#endif /* platformTimerDestroy */
#ifndef platformLog
#define platformLog(...) /*!< Log method */
#endif /* platformLog */
#ifndef platformAssert
#define platformAssert( exp ) /*!< Asserts whether the given expression is true */
#endif /* platformAssert */
#ifndef platformErrorHandle
#define platformErrorHandle() /*!< Global error handler or trap */
#endif /* platformErrorHandle */
#ifdef __cplusplus
}
#endif
#endif /* RFAL_PLATFORM_H */