Skip to main content
Visitor II
December 8, 2019
Solved

ST25R3911B-DISCO compliant tags

  • December 8, 2019
  • 1 reply
  • 579 views

I would like to find out if the eval board ST25R3911B-DISCO will be able to read the Avery Dennison RF700048 HF tag, which uses the NXP ICODE SLIX chip.

Thanks,

Narek

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi ,

    the ST25R3911B-DISCO Discovery kit for ST25R3911B can be operated as an ISO15693 reader thus the memory of the aforementioned tags can be read using the READ SINGLE BLOCK command as defined in ISO/IEC 15693-3.

    On PC side, you can use either the ST25R3911B Discovery GUI (STSW-ST25R001) or the ST25PC-NFC Windows® PC software (STSW-ST25PC001).

    Feel free to share more details about your application.

    Rgds

    BT

    1 reply

    Technical Moderator
    December 10, 2019

    Hi ,

    the ST25R3911B-DISCO Discovery kit for ST25R3911B can be operated as an ISO15693 reader thus the memory of the aforementioned tags can be read using the READ SINGLE BLOCK command as defined in ISO/IEC 15693-3.

    On PC side, you can use either the ST25R3911B Discovery GUI (STSW-ST25R001) or the ST25PC-NFC Windows® PC software (STSW-ST25PC001).

    Feel free to share more details about your application.

    Rgds

    BT