Skip to main content
Explorer
May 10, 2023
Solved

ST25R3911B-DISCO debugger connection

  • May 10, 2023
  • 1 reply
  • 787 views

I have a question, I don't know if 3911 in the image below is jtag download code or SWD.


_legacyfs_online_stmicro_images_0693W00000bjn3lQAA.png

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    P201 10-pin connector on ST253911B-DISCO is a JTAG/SWD interface to assist in software development on the onboard STM32L476RE. It can be connected to an external ST-LINK/V2 device using a 9-pin Cortex®-M adapter. See User Manual UM2042 for description of the ST253911B-DISCO and see STM32L476RE Reference manual RM0351 for details about the Single Wire/JTAG Debug Port.

    Rgds

    BT

    1 reply

    Technical Moderator
    May 10, 2023

    Hi,

    P201 10-pin connector on ST253911B-DISCO is a JTAG/SWD interface to assist in software development on the onboard STM32L476RE. It can be connected to an external ST-LINK/V2 device using a 9-pin Cortex®-M adapter. See User Manual UM2042 for description of the ST253911B-DISCO and see STM32L476RE Reference manual RM0351 for details about the Single Wire/JTAG Debug Port.

    Rgds

    BT