ST25R3911B ERROR FRAMING in reception
Hi,
i'm trying to perform a communication with an ISO14443-A smart card using the X-NUCLEO-NFC06A1 expansion board. The smart card supports the following bit rate: 106, 212, 424 and 848 kbit/s according to the ATS received. If i negotiate with the smart card a 848 kbit/s bit rate both in transmission and reception and i try to send an APDU, the rfal library returns an ERROR FRAMING in reception. In particular the error is returned by rfalTransceiveRx() method implemented in rfal_rfst25r3911.c file:
case RFAL_TXRX_STATE_RX_WAIT_RXE:
irqs = st25r3911GetInterrupt( (ST25R3911_IRQ_MASK_RXE | ST25R3911_IRQ_MASK_FWL | ST25R3911_IRQ_MASK_EOF) );
if( irqs == ST25R3911_IRQ_MASK_NONE )
{
/*******************************************************************************/
/* REMARK: Silicon workaround ST25R3911B Errata #1.1 */
/* ST25R3911 may indicate RXS without RXE afterwards, this happens rarely on */
/* corrupted frames. */
/* SW timer is used to timeout upon a missing RXE */
if( rfalTimerisExpired( gRFAL.tmr.RXE ) )
{
gRFAL.TxRx.status = ERR_FRAMING;
gRFAL.TxRx.state = RFAL_TXRX_STATE_RX_FAIL;
}
/*******************************************************************************/
break; /* No interrupt to process */
}It seems that the chip does not receive the end of frame and a timer interrupt occurs. If, instead, the bit rate is set to 424 kbit/s no problem occurs. Is there someone could explain me why this happens? Moreover, where i can find the ST25R3911B Errata #1.1?
Thanks in advance. Best regards,
Pierluigi