ST25R3911B Field Strengh Ratio
Hello,
I'm working with ST25R3911B and in my application i want to control the field strengh.
I relied on the documentation at this chapter : 1.3.40 RFO normal level definition register page 80 in the Datasheet - ST25R3911B - High performance HF reader / NFC initiator with 1.4 W supporting VHBR and AAT

And, if i understand well if i write 0x00 in the 0x27 register it will enable all Ohms segments, it will make 510 ohms.
If i write 0x01 510-256=254 right ?
But when I test my application with a field detectorit it doesn't seem to react as expected.
Am I doing something wrong ?
Best regards,
Yvan