Skip to main content
Visitor II
February 20, 2018
Solved

ST25R3911B SINGLE-ENDED CONFIGURATION EXAMPLES AVAILABLE?

  • February 20, 2018
  • 4 replies
  • 1875 views
Posted on February 20, 2018 at 02:22

The ST25R3911B datasheet, page 14 Figure 3, shows a minimum configuration of antenna connection components. There are provided schematics and layouts for the differential antenna configuration, however are there any recommended component values/layout available for the single ended configuration?

Datasheet: 

http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/ba/60/79/5c/bb/a9/41/76/DM00321525/files/DM00321525.pdf/jcr:content/translations/en.DM00321525.pdf

 

Application note: 

http://www.st.com/resource/en/application_note/dm00347152.pdf

 

#st25r391x #st25r3911b
    This topic has been closed for replies.
    Best answer by Travis Palmer
    Posted on March 01, 2018 at 16:20

    Hi Danyon,

    The ST25R3911B is capable of driving one differential antenna (using RFO1 and RFO2) or switching between two single ended antennas (one connected between RFO1 and GND the other to RFO2 and GND).

    Which RFO/RFI is used by the chip can then be selected by flipping the 'rfo2' register.

    These antennas could either be normal antennas (like the differential one) or 50Ohm antennas.

    50Ohm antennas are already foreseen with damping resistor, series and parallel capacitor to be tuned to 50Ohm at 13.56MHz. They can then be plugged using a 50Ohm coax cable to the NFC reader unit. In addition the NFC Reader unit requires a matching circuit to match the IC's load impedance seen on RFO1/2 to 50Ohm.

    The minimum load impedance for differential use is Zload = 8Ohm. (Datasheet Table 100) Therefore the minimum load impedance for single ended use would be Zload = 4Ohm.

    Since the target (50Ohm) is fixed, the matching values do not have to be changed when changing the antenna:

    For example:

    4Ohm to 50Ohm matching network:

    LEMC = 240nH

    CEMC = 330pF

    Cseries = 680pF

    Cpara = 270pF

    8Ohm to 50Ohm matching network:

    LEMC = 330nH

    CEMC = 220pF

    Cseries = 470pF

    Cpara = 180pF

    For conventional antennas (not matched to 50Ohm) the approach of finding the proper matching network is similar to what is described in the AN4974.

    You have to first measure the antenna parameter.

    Measured Antenna Parameters:

    Inductance @ 1MHz:    929nH

    DC resistance @ 1MHz:    329mOhm

    Parallel resistance @ SRF: 1500Ohm

    SRF:             62.667MHz

    To get the proper values for the single ended antennas you have to input twice the Antenna Inductance, DC resistance and Parallel resistance. The Self Resonance Frequency stays the same.

    The inputs into the 'ST25R Antenna Matching Tool' would then be:

    Inductance @ 1MHz:    1858nH

    DC resistance @ 1MHz:    658mOhm

    Parallel resistance @ SRF: 3000Ohm

    SRF:             62.667MHz

    Since the tool will calculate the circuitry for a differential matching network, we will have to input also twice the target impedance.

    The 'Matching inputs' would look like this:

    EMC Inductor: 270nH

    DC Resistance: 500mOhm

    EMC filter: 11750kHz

    Target matching Z: 16Ohm (this will give us 8Ohm for single ended use)

    Target antenna Q: 17

    After hitting 'calculate matching values' you will get reasonable results.

    Of course the matching inputs are subject to change - according to the AN4974 -

    Antenna

    matching

    for

    ST25R3911B/ST25R391x

    devices

    .

    BR Travis

    4 replies

    ST Employee
    March 1, 2018
    Posted on March 01, 2018 at 16:20

    Hi Danyon,

    The ST25R3911B is capable of driving one differential antenna (using RFO1 and RFO2) or switching between two single ended antennas (one connected between RFO1 and GND the other to RFO2 and GND).

    Which RFO/RFI is used by the chip can then be selected by flipping the 'rfo2' register.

    These antennas could either be normal antennas (like the differential one) or 50Ohm antennas.

    50Ohm antennas are already foreseen with damping resistor, series and parallel capacitor to be tuned to 50Ohm at 13.56MHz. They can then be plugged using a 50Ohm coax cable to the NFC reader unit. In addition the NFC Reader unit requires a matching circuit to match the IC's load impedance seen on RFO1/2 to 50Ohm.

    The minimum load impedance for differential use is Zload = 8Ohm. (Datasheet Table 100) Therefore the minimum load impedance for single ended use would be Zload = 4Ohm.

    Since the target (50Ohm) is fixed, the matching values do not have to be changed when changing the antenna:

    For example:

    4Ohm to 50Ohm matching network:

    LEMC = 240nH

    CEMC = 330pF

    Cseries = 680pF

    Cpara = 270pF

    8Ohm to 50Ohm matching network:

    LEMC = 330nH

    CEMC = 220pF

    Cseries = 470pF

    Cpara = 180pF

    For conventional antennas (not matched to 50Ohm) the approach of finding the proper matching network is similar to what is described in the AN4974.

    You have to first measure the antenna parameter.

    Measured Antenna Parameters:

    Inductance @ 1MHz:    929nH

    DC resistance @ 1MHz:    329mOhm

    Parallel resistance @ SRF: 1500Ohm

    SRF:             62.667MHz

    To get the proper values for the single ended antennas you have to input twice the Antenna Inductance, DC resistance and Parallel resistance. The Self Resonance Frequency stays the same.

    The inputs into the 'ST25R Antenna Matching Tool' would then be:

    Inductance @ 1MHz:    1858nH

    DC resistance @ 1MHz:    658mOhm

    Parallel resistance @ SRF: 3000Ohm

    SRF:             62.667MHz

    Since the tool will calculate the circuitry for a differential matching network, we will have to input also twice the target impedance.

    The 'Matching inputs' would look like this:

    EMC Inductor: 270nH

    DC Resistance: 500mOhm

    EMC filter: 11750kHz

    Target matching Z: 16Ohm (this will give us 8Ohm for single ended use)

    Target antenna Q: 17

    After hitting 'calculate matching values' you will get reasonable results.

    Of course the matching inputs are subject to change - according to the AN4974 -

    Antenna

    matching

    for

    ST25R3911B/ST25R391x

    devices

    .

    BR Travis

    Visitor II
    October 29, 2018

    Hello Travis,

    Could you provide us with a schematics (pdf) of the suggested implementation?

    Thanks and BR,

    Eric

    Visitor II
    September 30, 2018

    Hello Travis, I want to use standard 50 Ohm antenna with two outputs. What cable should I use for connection? Is coax cable is ok when using two outputs in differential mode or should i use shielded twisted pair?

    ST Employee
    October 2, 2018

    Hello Anatoly,

    Ideally a coax cable should be taken for single ended applications and shielded twisted pair with a defined characteristic impedance should be used for differential applications.

    BR Travis

    Visitor II
    October 2, 2018

    Thanks for the answer, Travis!