ST25R3911B single ended read range
Hello,
I'm currently working on a PCB prototype which uses the ST25R3911B as a front-end. I'm trying to handle multiple antennas in a time-multiplexed manner so i'm using both RFO pins and feeding them to RF switches (PE42421SCAA-Z, around 0.3-0.5 dB insertion loss) to further increase the number of available antennas.
I've used the ST25 antenna matching tool and the eDesignSuite as well to get a close match with a 10x10cm pcb antenna (2 turns,3mm traces, 2mm gap). For the first attempt I've managed to get a generous range of 15cm-s with ST25 nfc type 5 tags - matched to 4 Ohms - albeit with a 1 Ohm ESR 240 nH inductor .
Using the measure amplitude command I get around 1.4V as result.
My question is - would it be possible to increase this range with perhaps a larger single loop antenna and/or better matching? Should I perhaps modify the capacitive voltage divider on the RFI feedback to max out the 3V range - or it wouldn't matter? Or maybe use a lower ESR inductor? The target tags would be NFC type 5 of course. Thanks for the help in advance!
-Martin