ST25R3911B VDD Range
This seems like an "easy" topic, yet I'm struggling to get a clear understanding.
Section 3.2 of the datasheet (Operating Conditions) defines a single, wide range for VDD (2.4V to 5.5V). But Section 1.3.2 (IO Configuration Register 2) defines two non-contiguous VDD range (either 2.4V to 3.6V or 4.1V to 5.5V). Does this indicate that VDD between 3.6V and 4.1V is not supported?
Based on Section 3.2, we did a HW design where VDD is powered from a battery (3.3V to 4.2V) and we have an issue where sometimes the Adjust Regulator command fails to complete (no interrupt received within 10ms). And wondering if we are violating the supported VDD range.
I've also dug through RFAL001 and it looks like it sets sup3_V to 5V if VDD > 3.6V. This also indicates the VDD range from 3.6V to 4.1V is not supported because (in 5V mode) the minimum VSP_RF is 3.9V and VDD has to be about 0.25V higher.