ST25R3911B with FreeRTOS
Hi everybody,
I need to integrate the ST25R3911B NFC reader (X-NUCLEO-NFC05A1 a.t.m.) into a project with STM32H735G running FreeRTOS (with a TouchGFX task and another peripheral task running ).
https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/interfacing-st25r3911b-with-stm32f072-using-freertos/m-p/570845#M8893 following this old thread: I integrated https://www.st.com/en/embedded-software/stsw-st25r-lib.html library (latest release v1.5), put NFC ndef r/w demo inside a task with st25r3911Isr called inside EXTI0_IRQHandler and actually it works! But, of course, the SPI reading executed inside an IRQ is not efficient, in fact, other tasks don't work properly.
So now I'm trying to integrate the FreeRTOS_polling example, located in ST25R3916B / X-NUCLEO-NFC06A1 folder... it looks good to me but I can't get it working correctly, it instantly fails on the demoIni() where rfalNfcInitialize() returns 0x8 System Error.
Has anyone integrated FreeRTOS correctly with the module (it's ok under STM32L4, MCU porting doesn't seem to be a problem) in order to handle the irq like the example cited above? Do you have any suggestions?
Thanks for your time
Simone