ST25R3911B with VDD powered by 3.3V reports 0V for VDD, VSP_A, VSP_D & VSP_RF
I have ported the STM32F4 firmware written for NFC05A1 board and got it to run well on a Nucleo STM32F0 board.
Since then, I have since designed and prototyped a custom board with with the NFC05A1 reference design copied and controlled with an STM32F0.
The only difference between this board and my Nucleo paired evaluation board set-up is that I have 3.3V going to both VDD and VDD_IO of the ST25R3911B, unlike the reference design which has a VDD of 5V.
My design does not seem to be working properly, even though the SPI interface is working correctly and I can read/write registers.
I have noticed this:
When I run my firmware on the NFC05A1, I can read the correct values for the Power Supplies using the Measure Voltage command, ie:
VDD = 5.1V
VRF = 5.1V
VSA = 3..4V
VSD = 3.4V
BUT, when I run the same firmware on my board (even if I set the sup3_V bit in the IO Config Register 2), I get ZERO for all these 4 supplies.
Am I doing something wrong?
Do I need to change something in the reference firmware for the NFC05A1 to accommodate the VDD value of 3.3V?
Please advise.
Thanks.
Bob N