ST25R3916 Antenna Design Guidance?
I've created my own differential AAT board (3 turn 80x36mm antenna) that is working, but with a range of only 4cm compared to the NFC06A1 range of 8cm using a similar 15693 tag . With my own board powered off, I used my miniVNA to measure the matching network and antenna and see a minimum VSWR 2.365 and matching frequency of 16.52 MHz. When I measure the Nucleo NFC06A1 it yields a VSWR of 3.727 and a matching frequency of 13.3192. When I use QUCs to simulate my board with the same matching components its different (more capacitive on the smith chart). I was hoping the QUCS simulation would be more inline with what I'm seeing with the miniVNA. Which is more trustworthy, QUCS or the miniVNA for tweaking the matching network? I've attached some charts to show the differences. Any suggestions of how to proceed would be much appreciated. Thanks