ST25R3916 using AAT and Hardware wake-up
Hi, I have a issue with the ST25R3916 when using the AAT and the Hardware wake up functions together.
The tuning works fine and finds the best parameters, then when entering sleep mode the parameters changes to a fixed value. When waking up the first time the outputs for aat_a and aat_b goes back the tuning parameters, but every wake up after outputs for aat_a and aat_b are just 2V.
How can I get the ST25R3916 to use the tuning parameters every time?
And why does ST not recommend using these two features together?
I have looked in the example projects for the IC but there the AAT is not used.
Below some scope images of the AAT_B output (Yellow, green is data transfer).
AAT with an antenna with capacitance and the first card read.
AAT of antenna with high capacitance
First and second card read of antenna with high capacitance.
Also if any have a quick explanation/link to an note of why the voltage always is at 1.5V every time there is data transfer (Green line). I will appreciate that as well.