Skip to main content
Visitor II
May 22, 2024
Solved

ST25R3916B output slew rate

  • May 22, 2024
  • 1 reply
  • 936 views

Is it possible to adjust the slew rate of the RFO1/RFO2 outputs of the ST25R3916B?

    This topic has been closed for replies.
    Best answer by Ulysses HERNIOSUS

    Hi,

    that is all information that I can offer. Just set d_tim_man=1 and cycle through the 5 d_tim values turn on the field and see if you observe a change.

    BR, Ulysses

    1 reply

    Technical Moderator
    May 23, 2024

    Hi,

    what are you trying to achieve with changing the slew rate?

    Driver behavior can be influenced by means of the bits in Tx Driver Timing Register (B 29h).

     

    BR, Ulysses

    TM1Author
    Visitor II
    May 23, 2024

    I'd like to explore the possibility of reducing rise and fall time of the Tx outputs to reduce harmonics.  (This would be in addition to correct EMC filter values, proper layout, optimization of AAT range per AN5322, etc.)

    I see the Tx driver timing register described in section 4.5.51 of the datasheet, but there's not a lot of detail.  Where can I find more information?

    Technical Moderator
    May 23, 2024

    Hi,

    that is all information that I can offer. Just set d_tim_man=1 and cycle through the 5 d_tim values turn on the field and see if you observe a change.

    BR, Ulysses