ST25R3916B Passive Target Sample Code
Is there any example code for ISO14443A passive target mode, which is supported on the ST25R3916B? I'm prototyping basic functionality before fully implementing our application, and it would be nice to do a proof of concept without having to grapple with the RFAL. I'm using the X-NUCLEO-NFC08A1 with an STM32L476RG_NUCLEO.
To that note, if there are any instructions on using the RFAL (which headers to modify, any other configurations to set), I would appreciate being pointed to them.