ST25R3916B RF power output
Hi, it's not clear the deliverable power of the ST25R3916B. it seems 1.6W in balance output configuration. On the datasheet is written only that there is a dynamic power output, on the first page then no more other information, and there are no registers about the output power it seems..
I have to do a connection P2P between 2 eval NUCLEO-NFC08A1, but i get only 9cm of maximum distance range. it's a poor result for 1.6W...
is there the possibility to control manually the power output?
how is it possible to increse the distance range in P2P mode (without changing the antenna)?
i'm waiting your reply soon
thanks
Logantenna