ST25R3920B NDEF Handover Record (Bluetooth OOB Pairing)
Hello everyone,
I am currently using a custom NFC board based on the X-Nucleo-NFC08A1 that has the ST25R3920B MCU. I am able to perform OOB pairing (LE Secure Connections) using the example provided by ST in the software tools example. I can sucessfuly complete the bluetooth pair using a Samsung A12, however if I use other smartphones like Google Pixel 6, Xiaomi 14T or even Huawei the pairing does not complete.
I have tried this with other manufacturers libraries and software and it works for all the smartphones. After inspecting the memory of the tag I found out they use a "Handover Select" record with an "Alternative Carrier" inside. I dont't know if this is why it is not working with other smartphones.
Could someone explain this better, and if so, how do I set this additional records?
Best regards.