(ST25R3920B) RFAL_ERR_SYSTEM error in ST25R_SELFTEST_TIMER macro
Hi,
Now I am trying to port the rfal library for an ST25R3920B.
I have defined all mandatory part of platform.h and rfal_defConfig.h file.
And I enabled the flags ST25R_SELFTEST, ST25R_SELFTEST_TIMER to find out issues of initializing.
The ST25R_SELFTEST is passed without any error, but for ST25R_SELFTEST_TIMER it fails in st25r3916WaitForInterruptsTimed function
st25r3916EnableInterrupts( ST25R3916_IRQ_MASK_GPE );
st25r3916SetStartGPTimer( (uint16_t)ST25R3916_TEST_TMR_TOUT_8FC, ST25R3916_REG_TIMER_EMV_CONTROL_gptc_no_trigger);
if( st25r3916WaitForInterruptsTimed( ST25R3916_IRQ_MASK_GPE, (ST25R3916_TEST_TMR_TOUT - ST25R3916_TEST_TMR_TOUT_DELTA)) != 0U )
{
platformErrorHandle();
return RFAL_ERR_SYSTEM;
}
And then, I looked closely at the if conditional sentence, and I don't understand it.
The return value of st25r3916WaitForInterruptsTimed() function is not 0 when an interrupt occured without a timeout. right?
So it means when it's an abnormal state, return is zero...
I don't understand why it's an error when the st25r3916WaitForInterruptsTimed() output value is not zero.
Is there something wrong with my understanding? If so, please let me know
best regards,