ST25R95 0x87 Response from SENDRECV
I am in the final stretch of my project using the ST25R95 with an ATTINY88. I am working on custom hardware and not using libraries.
I have all of the ST25R95 related commands working on my development setup with an Arduino UNO and X-NUCLEO-NFC03A1 but I moved to the custom hardware and I am not able to read a tag.
I used the EMI Filter Calculator to determine the values for the EMI filter and matching circuit. Measuring with a spectrum analyzer, I have a higher level of output at 13.56 MHz than the NUCLEO dev board. So my matching must be pretty good.
I have attached the SPI trace from boot to the SENDRECV REQ command to wake the ISO14443-A tag but I get a 0x87 response.
Any ideas?