Skip to main content
Graduate
February 26, 2024
Solved

ST25R95 Jumps out of IDLE without tag

  • February 26, 2024
  • 4 replies
  • 2561 views

Using my Arduino UNO and X-NUCLEO-NFC03A1 with the ST25R95 I am having issues trying to stay in IDLE.

For DacDataL and DacDataH, I have tried both the recommended 0x64 and 0x74 for the demo board and the 0x90 and 0xA0 that came from Tag Detection Calibration.

Approximately every 552ms it jumps out of Idle state and the IRQ_O never goes LOW.

I have attached a trace.  I still haven't been able to capture a trace that includes IRQ_O.

It shows boot, going into Idle, jumps out of Idle, polls for reading, reads and goes back to Idle.

Why might my code be jumping out of Idle mode?

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    I've seen a protocolSelect ISO14443A in your trace before going to Idle. Make sure the field is OFF before going to Idle mode (ie. send a 00 02 01 00 = protocolSelect FieldOff ).

    The IRQ_OUT returns high when the response from the device has been read. Therefore, before sending a new command, the response of the previous one has to be read.

    Can you share a picture of your HW setup? Is the X-NUCLEO-NFC03A1 antenna covering some electronics part of the Arduino board?

    Rgds

    BT

    4 replies

    Technical Moderator
    February 26, 2024

    Hi,

    As explained in the ST25R95 datasheet §5.9, the SPI poll mechanism cannot be used when the device is in WFE mode and the application has to rely on the IRQ_OUT. 

    In the trace, I can see a SPI Poll after then Idle command. Its response has no meaning. Only the IRQ_OUT should be used.

    I've also seen that the poll command does not follow figure 7 § 4.1.1 of the datasheet. I would suggest to use only IRQ_OUT in the whole application as this is done inside the RFAL.

    Rgds

    BT

    PDIhawkAuthor
    Graduate
    February 26, 2024

    Hi Brian,

    I'm aware of datasheet §5.9 and I'm not using the SPI poll mechanism in that manner.

    The poll that you are seeing runs after it jumps out of idle because it thinks that it sees a tag and tries to do a read.

    I commented out the poll and read.  The attached log is from a version that boots, goes into Idle, waits for IRQ_O to go LOW, IRQ_O goes low and goes back to idle.  Unfortunately, it looks like it IRQ_O never goes HIGH again because I'm not reading out the part anymore.

    Looking back over my code, this was a branch of my original code from before I could calibrate or read a tag. This branch is specifically to get Idle working.  So the tag reading commands were not complete but I don't think that adding those routines would have an effect on this issue.

    Regardless, I will move to using IRQ_O instead of an SPI polling routine for reads.

    Thanks!

    -Andrew

    Technical Moderator
    February 26, 2024

    Hi,

    I've seen a protocolSelect ISO14443A in your trace before going to Idle. Make sure the field is OFF before going to Idle mode (ie. send a 00 02 01 00 = protocolSelect FieldOff ).

    The IRQ_OUT returns high when the response from the device has been read. Therefore, before sending a new command, the response of the previous one has to be read.

    Can you share a picture of your HW setup? Is the X-NUCLEO-NFC03A1 antenna covering some electronics part of the Arduino board?

    Rgds

    BT

    Technical Moderator
    February 26, 2024

    Hi,

    do you mean that after a command, you start a 100ms timer and wait for either IRQ_OUT (ie. response available) or timer expiry?

    This would be helpful to have an SPI trace with IRQ_IN and IRQ_OUT so that I can check the startup sequence timings. In particular, make sure to properly wait for t3 after the initial IRQ_IN pulse. See https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/cr95hf-error-0x71-spi-interface/m-p/329870 for an example of initialization sequence. Before sending the echo command, it is possible to poll for readiness by sending a poll control byte (0x03) after the startup sequence (i.e. after t3), If bit2 of the response byte is 1, the CR95HF is ready to receive commands. When sending the poll control byte to poll for readiness after startup, the usual response is 0x06 which means a command such as echo can be sent to the ST25R95.

    Rgds

    BT

    PDIhawkAuthor
    Graduate
    February 26, 2024

    Ok, after closer looking at the ST32duino library code, I was missing an nIRQ Pulse on boot.  I had the one after reset but not on boot as I should have.

    After turning the Field OFF before Idle and adding the nIRQ Pulse before the Reset command, my problems above are fixed.

    Now I can't seem to get it to recognize a tag, but I guess that is for another thread.

    Technical Moderator
    February 26, 2024

    Well done!