ST25R95 poor reception
I have this board with a large (91x119mm) surrounding it. There is circuitry including the ST25R95 in the middle, but it has quite some clearance to the antenna. Matching network is calculated using the ST excel sheets.
Now I can get it to read NFC stickers, but only if I put them right on the matching network. Before I do a big investigation into the antenna and matching network, what are the parameters I can adjust in the ST25R95 that effect reception strength?
I see chapter 5.1.1 in the datasheet " Improving RF performance " mention Modulation index and receiver gain. Are those the two parameters I should be looking at? Are there more?