Skip to main content
Visitor II
June 23, 2020
Solved

ST25R95 - RF matching component selection, according to my drawing of NFC antenna/coil

  • June 23, 2020
  • 1 reply
  • 724 views

Hi all.

I am going to make a complete prototype of a PCB which include NFC transceiver ST25R95. I Have calculated with ST spreadsheets the values of matching capacitors from estimated values of Rant and Lant, Cant is unknown and is not being considered. The measures, I mean from one hole to another hole, the coil/antenna. The coil is drawn on both sides of the PCB.

Current schematic of RF part:

0693W000001rFItQAM.png

Current PCB layout:

0693W000001rFIyQAM.png0693W000001rFJ3QAM.png

eDesign tool gives Lant = 567nH. Since the coil is double side, multiply it by 4 (but I will use 3.75). Then, 3.75 * 567nH = 2.13uH.

0693W000001rFJcQAM.png

So I drawn the coil. Total lenght is 594mm, if consider both sides summed. Rant calculated = 2.05 ohms. To reach 2.05 ohms, use PCB parameters: 0.5 oz (18um) copper thickness, length = 594mm total and 12 mils for trace width.

Having Rant = 2.05 ohms and Lant = 2.13uH, I can use the component calculator spreadsheet of ST25R95. And from here came my values shown at the top of the topic for capacitors C21, C22 and C23.

0693W000001rFL4QAM.png

Is there something missing on the calculations or on the procedure? For example I don't know how to calculate the capacitance between the holes, maybe it should be considered...

PCB thickness is 1.6mm.

And on layout software the antenna looks like this:

0693W000001rFKuQAM.png

Considering that antenna, could I choose more suitable values than the ones that are currently choosen?

Regards.

    This topic has been closed for replies.
    Best answer by Henry Crane

    ​Hello,

    the procedure you followed is the right one.

    just for commentsing:

    • your  antenna coil extraction from one layer to 2 layer is right except that multiplying the single layer coil inductance by 4 correcponds to ideal case of coupling factor between layers is 1. Generally, the signle layer coil inductance shall be multiplied by something between 3 and 4. this leads to a range of compionent values instead of fixed ones.
    • Edesign suite antenna modules calculates the coil inductance taking into account the parasitic cap. thus, value given by eDesign suite is closer to the equivalent inductance extracted from imaginary part of impedance rather than the pure self inductance. so no need to hole to home capacitance.
    • last point, as described in AN5248 calculated components shall be validated by a tuning circuit input impedance session.

    feel free to tell us if you need help for this.

    Best regards,

    Henry Crane

    NFC/RFID technical support

    1 reply

    ST Employee
    June 25, 2020

    ​Hello,

    the procedure you followed is the right one.

    just for commentsing:

    • your  antenna coil extraction from one layer to 2 layer is right except that multiplying the single layer coil inductance by 4 correcponds to ideal case of coupling factor between layers is 1. Generally, the signle layer coil inductance shall be multiplied by something between 3 and 4. this leads to a range of compionent values instead of fixed ones.
    • Edesign suite antenna modules calculates the coil inductance taking into account the parasitic cap. thus, value given by eDesign suite is closer to the equivalent inductance extracted from imaginary part of impedance rather than the pure self inductance. so no need to hole to home capacitance.
    • last point, as described in AN5248 calculated components shall be validated by a tuning circuit input impedance session.

    feel free to tell us if you need help for this.

    Best regards,

    Henry Crane

    NFC/RFID technical support