ST25RU3993_EVAL firmware will not work on Rain board
I am trying to test the ST25RU3993_Eval code and .ioc project with the ST25RU3993 Rain Board. I have uploaded the ST25RU3993_eval.bin through the firmware update option under help on the ST25RU3993 Reader Suite, but the board does not recognize it, and gives the error it isn't compatible.
Why is this firmware failing, as it was my understanding this was a compatible firmware for the Rain Board? The project builds correctly within the STMCubeIDE, but the bin file produced will not work as firmware through the suite.
Is there a way to get a hold of the .ioc files for the only firmware that works for the READER? The only firmware I get to work on the RAIN Reader Suite is ST25RU3993_FW_v3-0-0-0_Eval.bin.
Thanks