Dear Fma.1,
thanks, I thing I understand the situation your are facing.
What I am trying to explain is that you should check if the tag is responding at distances >4 m.
I acknowledge that I have assumed that the concept how to do this was clear and therefore did not explain it in detail.
So while the reader is scanning for tags, place the tag at a distance >4m.
At the same time you could check with a second antenna, that is for instance connected to a spectrum analyzer, if a tag response is present.
You could check this in the frequency or in the time (zero-span) domain.
- If you see a tag response happening then it would mean the reader's sensitivity is to low.
- If there is no tag response and you see only the reader's modulated spectrum then the tag has most probably insufficient power to turn ON.
Your observation that at 3.5m the tag can be detected only for ten seconds might be an indication that the tag has insufficient power.
A possible explanation is that when the reader starts to operate (and the reader is cold), TX power is the highest.
When the reader continues to operate is gets warm the TX power drops a little bit.
Maybe at 3.5m the tag is marginally powered and just a bit less TX power shuts the tag OFF.
You could also place the tag at 3.5m and slightly reduce the TX power in the reader settings. If the tag is then never responding at all it indicates that TX power is responsible.
I hope this explanation was helpful to you.
Cheers,
B