Skip to main content
Visitor II
March 3, 2023
Solved

ST25RU3993s with marking "E"

  • March 3, 2023
  • 1 reply
  • 1871 views

I have ST25RU3993s with marking "E". I see a note in rev.11 datasheet mentioned not to used the "E" or "ES" marking for the production board.

(1)Is the note still true?

(2)If It's released in the field, what kind of failures do I expect?

Thanks,

-Tieng

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Now the problem becomes a little clearer: it is pretty sure that the marking E is not engineering samples and also not a chip revision.

    I don't have the exact details at the moment but hopefully the OLS team do, please open a ticket there and informally ask in the text to add your contact at the distributor so they are informed as well.

    Regards

    /Peter

    1 reply

    Technical Moderator
    March 3, 2023

    Welcome, @TNguy.50​, to the community!

    Correct, this statement is still valid and reads:

    Parts marked as “ES�?, “E�? or accompanied by an Engineering Sample notification letter, are not yet qualified and therefore not yet ready to be used in production and any consequences deriving from such usage will not be at ST charge. In no event, ST will be liable for any customer usage of these engineering samples in production. ST Quality has to be contacted prior to any decision to use these Engineering samples to run qualification activity.

    ST cannot and will make a statement about possible misbehaviour or failures.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter

    TNguy.50Author
    Visitor II
    March 3, 2023

    Hi Peter,

    As a follow-up, my factory receives a tape of ST25RU3993s which is mixed of rev B and rev E from the Future distributor, see attachment. (1) Is it a normal for a rev E (engineering samples) to mix with a released rev B in the same tape? (2) Also, what are rev [“A", "B", "C", "K", "G", "H" ] are being shipped by ST to our factory's distributors like Future in China?

    -Tieng

    Graduate II
    March 4, 2023

    @Peter BENSCH​ are we sure these designators here aren't simply assembly line identification marks. It would be very odd for a tape to contain sample and production parts.