ST28R3911B - RFAL Middleware : ERR_PROTO (11) Response when sending APDU Command
Where to I start to debug the RFAL middleware if I receive ERR_PROTO (11) when I call err= rfalIsoDepStartApduTransceive(P); or rfalIsoDepGetApduTransceiveStatus();
I receive ERR_PROTO from the RFAL when I send a card a specific (APDU) , For some cards it works and for others it doesn't. The only thing that I think could be the problem ( By looking at the responses from another NFC reader) is that it works when the response message is smaller than 128 bytes. Cards with R-APDU response lengths of 77 bytes work, but when I use a card that should return 133 bytes (R-APDU), I get the Error message (ERR_PROTO) from the function rfalIsoDepGetApduTransceiveStatus();