Stability issue with windows 10 gui version 1.2.2. How can I get version 1.1.22?
I have 3 of the ST25R3911B-Disco boards and they are working great with discovery gui version 1.1.22.0 on a windows 10 pro machine. I needed to set up a second pc and can now only get the gui version 1.2.2 when I try to connect to the new version I first had to upgrade my boards according to the new gui. But I could not do this using the version 1.2.2 it keep failing. I used my gui version 1.1.22 and was able to update the board with the 1.2 version firmware but when I try to use the version 1.2 gui it works a couple times then gives me a packet info error and drops out. If I connect the board with the 1.2 firmware to the gui with the 1.1.22 everything is good. Any ideas on what he issue could be? How can I get the gui version 1.1.22 since is seems to work better than the new version?