STEVAL-25R200SA Antenna parameters in ST25R Antenna Matching Tool
Dear..ST
I'm developing custom NFC PCB 4 layers 0.8mm based on 20x20mm main antenna example in STEVAL-25R200SA kit.
I tried to use the components in BOM for EMC filter L 0402DF-421XJRW 420nH 510mOhm and adjust frequency to
18MHz and get EMC capacitor 186pF which is similar to the kit (180pF) I follow AN6065 as much as I understand.
However I don't know the Antenna parameters, Q value, of the kit, so the matching L, C, R seems not the same as the kit. So if you have these parameters, or smith chart of the main 20x20mm antenna, please share to me.
My application need very low power and the distance of the ST25DV64 tag and the reader is very close (5-10mm).
I will try to tune antenna for lowest current consumption so that the reader still read the tag.
Please advise Target Q, and Target matching Z, I should use with 20x20mm antenna.
The supply for the ST25R200 is 3.3V
(I read AN13219 from NXP as well, page 22 noted that Target Z 16 Ohm for 5V, 11 Ohm for 3.3V so I guess to reduce Target Z for lower supply?)
In addition, I found that Coilcraft 0402DF-421XJRW cannot buy easily and very expensive compared to other series.
Is document AN6065 antenna parameters in tool based on X-NUCLEO-NFC10A1 or N-NUCLEO-NFC09A1?
Both kits has the same antenna, but why the L, C matching circuit are not the same and not as in AN6065 tool?
Thanks in advance.