Skip to main content
Explorer II
December 18, 2023
Solved

STEVAL-SMARTAG2 - Error: failed to erase memory

  • December 18, 2023
  • 2 replies
  • 1227 views

I am trying to update the firmware in the STEVAL-SMARTAG2 using Memory & File editing  in STM32 CubeProgrammer Windows Application., but I get Error: failed to erase Memory.

My goal is to install your demo firmware to use the SMARTAG2 with ST NFC Sensor Mobile app.

Screen shots and the Log, Verbosity level 3 follow.

Note I have Rev A of the SMARTAG2 

Thanks,

Vince

Screenshot (3073).pngScreenshot (3075).pngScreenshot (3076).png

IMG_0292.jpg

    This topic has been closed for replies.
    Best answer by VColi.1

    BT,

    Thank you for that suggestion.  Yes putting a new battery fixed the problem (I can now Erase the Memory and add new firmware).

    Is there any App Note exapling how to install the demo firmware and then configure the sensors to work with the ST NFC Sensor Mobile App?

    Vince

    Screenshot (3509).png

    2 replies

    Technical Moderator
    December 18, 2023

    Hi,

    just a suggestion: is the battery (CR2032/LIR2032) providing enough energy?

    Rgds

    BT

    VColi.1AuthorAnswer
    Explorer II
    December 18, 2023

    BT,

    Thank you for that suggestion.  Yes putting a new battery fixed the problem (I can now Erase the Memory and add new firmware).

    Is there any App Note exapling how to install the demo firmware and then configure the sensors to work with the ST NFC Sensor Mobile App?

    Vince

    Screenshot (3509).png

    Technical Moderator
    December 19, 2023

    Hi,

    see User Manual  UM3034 Getting started with the STEVAL-SMARTAG2 NFC dynamic tag sensor and processing node evaluation board.

    If you have new questions regarding the STEVAL-SMARTAG2, I would recommend to create a new post rather than reusing this one which is related to a battery issue.

    Thanks

    Rgds

    BT